RPL parameter set.
Public Attributes#
Amount of time a parent should retain a registered GUA/ULA (seconds)
RPL max candidate parents.
RPL first DIS maximum delay (seconds)
RPL DIS maximum delay (seconds)
Maximum period of NS probes used to get samples for ETX calculation (seconds)
Number of samples used to calculate ETX during join state 4.
Number of samples used to refresh ETX.
Delay for preferred parent selection after first DIO reception (seconds)
RPL max parents.
Public Attribute Documentation#
address_registration_lifetime_s#
uint16_t sl_wisun_params_rpl::address_registration_lifetime_s
Amount of time a parent should retain a registered GUA/ULA (seconds)
145
of file /mnt/raid/workspaces/ws.wIWINzxl8/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h
candidate_parents_max#
uint8_t sl_wisun_params_rpl::candidate_parents_max
RPL max candidate parents.
151
of file /mnt/raid/workspaces/ws.wIWINzxl8/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h
dis_max_delay_first_s#
uint16_t sl_wisun_params_rpl::dis_max_delay_first_s
RPL first DIS maximum delay (seconds)
137
of file /mnt/raid/workspaces/ws.wIWINzxl8/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h
dis_max_delay_s#
uint16_t sl_wisun_params_rpl::dis_max_delay_s
RPL DIS maximum delay (seconds)
139
of file /mnt/raid/workspaces/ws.wIWINzxl8/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h
etx_probe_period_max_s#
uint16_t sl_wisun_params_rpl::etx_probe_period_max_s
Maximum period of NS probes used to get samples for ETX calculation (seconds)
143
of file /mnt/raid/workspaces/ws.wIWINzxl8/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h
etx_samples_init#
uint8_t sl_wisun_params_rpl::etx_samples_init
Number of samples used to calculate ETX during join state 4.
147
of file /mnt/raid/workspaces/ws.wIWINzxl8/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h
etx_samples_refresh#
uint8_t sl_wisun_params_rpl::etx_samples_refresh
Number of samples used to refresh ETX.
149
of file /mnt/raid/workspaces/ws.wIWINzxl8/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h
init_parent_selection_s#
uint16_t sl_wisun_params_rpl::init_parent_selection_s
Delay for preferred parent selection after first DIO reception (seconds)
141
of file /mnt/raid/workspaces/ws.wIWINzxl8/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h
parents_max#
uint8_t sl_wisun_params_rpl::parents_max
RPL max parents.
153
of file /mnt/raid/workspaces/ws.wIWINzxl8/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h