LFN power parameters.
Public Attributes#
uint8_t
If true, the LFN wakes up only for broadcast slots containing synchronization information.
uint16_t
Minimum duration of the listening window.
uint8_t
Reserved, set to zero.
uint16_t
Minimum margin added to the listening window (before and after).
Public Attribute Documentation#
broadcast_lts_only#
uint8_t sl_wisun_lfn_params_power_t::broadcast_lts_only
If true, the LFN wakes up only for broadcast slots containing synchronization information.
If false, the node wakes up on every LFN broadcast slot.
Definition at line
108
of file /mnt/raid/workspaces/ws.wIWINzxl8/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_lfn_params_api.h
listening_window_min_us#
uint16_t sl_wisun_lfn_params_power_t::listening_window_min_us
Minimum duration of the listening window.
Applies to both Unicast and Broadcast slots.
Definition at line
101
of file /mnt/raid/workspaces/ws.wIWINzxl8/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_lfn_params_api.h
reserved#
uint8_t sl_wisun_lfn_params_power_t::reserved[3]
Reserved, set to zero.
Definition at line
110
of file /mnt/raid/workspaces/ws.wIWINzxl8/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_lfn_params_api.h
window_margin_min_us#
uint16_t sl_wisun_lfn_params_power_t::window_margin_min_us
Minimum margin added to the listening window (before and after).
The real margin increases with aging synchronization info.
Definition at line
104
of file /mnt/raid/workspaces/ws.wIWINzxl8/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_lfn_params_api.h