LFN parent parameter set.

Public Attributes#

uint8_t

Number of broadcast LFN Pan Config retries when LFN Version is incremented Referred to as LFN_MAINTAIN_PARENT_TIME in FAN TPS 1.1.

uint8_t

Reserved, set to zero.

Public Attribute Documentation#

lfn_lpc_retry_count#

uint8_t sl_wisun_params_lfn_parent::lfn_lpc_retry_count

Number of broadcast LFN Pan Config retries when LFN Version is incremented Referred to as LFN_MAINTAIN_PARENT_TIME in FAN TPS 1.1.


Definition at line 178 of file /mnt/raid/workspaces/ws.wIWINzxl8/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h

reserved#

uint8_t sl_wisun_params_lfn_parent::reserved[3]

Reserved, set to zero.


Definition at line 180 of file /mnt/raid/workspaces/ws.wIWINzxl8/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h