Public Attributes#

int8_t

Db (negative) or EListenBeforeTalkThreshold_t.

Db (negative) or EtxPowerLevel_t.

Db (negative) or EtxPowerLevel_t.

int16_t

Maximum transmission power for Z-Wave LR.

RF Region setting.

uint8_t

Enable radio PTI.

Public Attribute Documentation#

iListenBeforeTalkThreshold#

int8_t SRadioConfig_t::iListenBeforeTalkThreshold

Db (negative) or EListenBeforeTalkThreshold_t.


Definition at line 1653 of file /mnt/raid/workspaces/ws.ZFSvPe7ik/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h

iTxPowerLevelMax#

zpal_tx_power_t SRadioConfig_t::iTxPowerLevelMax

Db (negative) or EtxPowerLevel_t.


Definition at line 1654 of file /mnt/raid/workspaces/ws.ZFSvPe7ik/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h

iTxPowerLevelAdjust#

zpal_tx_power_t SRadioConfig_t::iTxPowerLevelAdjust

Db (negative) or EtxPowerLevel_t.


Definition at line 1655 of file /mnt/raid/workspaces/ws.ZFSvPe7ik/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h

iTxPowerLevelMaxLR#

int16_t SRadioConfig_t::iTxPowerLevelMaxLR

Maximum transmission power for Z-Wave LR.


Definition at line 1656 of file /mnt/raid/workspaces/ws.ZFSvPe7ik/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h

eRegion#

zpal_radio_region_t SRadioConfig_t::eRegion

RF Region setting.


Definition at line 1657 of file /mnt/raid/workspaces/ws.ZFSvPe7ik/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h

radio_debug_enable#

uint8_t SRadioConfig_t::radio_debug_enable

Enable radio PTI.


Definition at line 1658 of file /mnt/raid/workspaces/ws.ZFSvPe7ik/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h