Public Attributes#
void(*
Placeholder for callback function Will be returned with transmit status Allows application to recognize frames.
uint8_t
Public Attribute Documentation#
Handle#
void(* SSendSucNodeId::Handle) (void)
Definition at line
1415
of file /mnt/raid/workspaces/ws.ZFSvPe7ik/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h
DestNodeId#
node_id_t SSendSucNodeId::DestNodeId
Placeholder for callback function Will be returned with transmit status Allows application to recognize frames.
Definition at line
1418
of file /mnt/raid/workspaces/ws.ZFSvPe7ik/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h
TransmitOptions#
uint8_t SSendSucNodeId::TransmitOptions
Definition at line
1419
of file /mnt/raid/workspaces/ws.ZFSvPe7ik/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h