AES-CMAC#
API and Callbacks for the AES-CMAC Component.
Silicon Labs implementation of AES-CMAC. See AN875 for more information.
API#
void
emberAfPluginAesMacAuthenticate(const uint8_t *key, const uint8_t *message, uint8_t messageLength, uint8_t *out)
Compute the Cipher-based Message Authentication Code (CMAC) corresponding to the passed message and the passed key.
API Documentation#
emberAfPluginAesMacAuthenticate#
void emberAfPluginAesMacAuthenticate (const uint8_t * key, const uint8_t * message, uint8_t messageLength, uint8_t * out)
Compute the Cipher-based Message Authentication Code (CMAC) corresponding to the passed message and the passed key.
Parameters
[in] | key | The key to be used to produce the cipher-based authentication code. |
[in] | message | A pointer to the message for which a cipher-based authentication code should be computed. |
[in] | messageLength | The length in bytes of the message to be authenticated. |
[out] | out | A pointer to a 16-byte area memory in which the resulting cipher-based authentication code will be stored. |
Definition at line
68
of file app/framework/plugin/aes-cmac/aes-cmac.h
Macro Definition Documentation#
initToConstZero#
#define initToConstZeroValue:
do \
{ \
MEMSET(x, 0x00, 16); \
} while (0)
Definition at line
36
of file app/framework/plugin/aes-cmac/aes-cmac.h
initToConstRb#
#define initToConstRbValue:
do \
{ \
MEMSET(x, 0x00, 15); \
x[15] = 0x87; \
} while (0)
Definition at line
42
of file app/framework/plugin/aes-cmac/aes-cmac.h