Modules#

Network Creator

Network Creator#

API and Callbacks for the Network Creator Component.

This component performs the necessary steps to create a network according to the Base Device Behavior specification. The component performs an active scan followed by an energy scan across a primary channel set to decide which channel(s) are valid candidates for network formation. If the component fails to form a network on any primary channels, it moves to a secondary channel mask. Before every attempt at network formation, this component sets up the stack to use Zigbee 3.0 security.

API#

EmberStatus
emberAfPluginNetworkCreatorStart(bool centralizedNetwork)

Command the network creator to form a network with the following qualities.

void

Stop the network creator process.

EmberStatus
emberAfPluginNetworkCreatorNetworkForm(bool centralizedNetwork, EmberPanId panId, int8_t radioTxPower, uint8_t channel)

Command the network creator to form a centralized network.

API Documentation#

emberAfPluginNetworkCreatorStart#

EmberStatus emberAfPluginNetworkCreatorStart (bool centralizedNetwork)

Command the network creator to form a network with the following qualities.

Parameters
N/AcentralizedNetwork

Whether or not to form a network using centralized security. If this argument is false, a network with distributed security will be formed.

Returns

  • Status of the commencement of the network creator process.


Definition at line 69 of file app/framework/plugin/network-creator/network-creator.h

emberAfPluginNetworkCreatorStop#

void emberAfPluginNetworkCreatorStop (void )

Stop the network creator process.

Parameters
N/A

Stops the network creator formation process.


Definition at line 75 of file app/framework/plugin/network-creator/network-creator.h

emberAfPluginNetworkCreatorNetworkForm#

EmberStatus emberAfPluginNetworkCreatorNetworkForm (bool centralizedNetwork, EmberPanId panId, int8_t radioTxPower, uint8_t channel)

Command the network creator to form a centralized network.

Parameters
N/AcentralizedNetwork

Indicates whether or not to form a network using centralized security. If this argument is false, a network with distributed security will be formed.

N/ApanId

The pan ID of the network to be formed.

N/AradioTxPower

The TX power of the network to be formed.

N/Achannel

The channel of the network to be formed.

Commands the network creator to form a centralized or distributed network with specified PAN ID, TX power, and channel.

Returns

  • Status of the commencement of the network creator process.


Definition at line 92 of file app/framework/plugin/network-creator/network-creator.h

Variable Documentation#

emAfPluginNetworkCreatorPrimaryChannelMask#

uint32_t emAfPluginNetworkCreatorPrimaryChannelMask

Definition at line 49 of file app/framework/plugin/network-creator/network-creator.h

emAfPluginNetworkCreatorSecondaryChannelMask#

uint32_t emAfPluginNetworkCreatorSecondaryChannelMask

Definition at line 50 of file app/framework/plugin/network-creator/network-creator.h

Macro Definition Documentation#

EMBER_AF_PLUGIN_NETWORK_CREATOR_PLUGIN_NAME#

#define EMBER_AF_PLUGIN_NETWORK_CREATOR_PLUGIN_NAME
Value:
"NWK Creator"

Definition at line 44 of file app/framework/plugin/network-creator/network-creator.h