Modules#
EmberAfFileDescriptorDispatchStruct
File Descriptor Dispatch#
API and Callbacks for the File Descriptor Dispatch Component.
This plugin provides an API to register a file descriptor and a callback that is called when the select() function notifies the plugin there is data on that file descriptor.
API#
EmberStatus
emberAfPluginFileDescriptorDispatchAdd(EmberAfFileDescriptorDispatchStruct *dispatchStruct)
EmberStatus
emberAfPluginFileDescriptorDispatchWaitForEvents(uint32_t timeoutMs)
bool
emberAfPluginFileDescriptorDispatchRemove(int fileDescriptor)
Enumerations#
enum
EMBER_AF_FILE_DESCRIPTOR_OPERATION_NONE = 0x00
EMBER_AF_FILE_DESCRIPTOR_OPERATION_READ = 0x01
EMBER_AF_FILE_DESCRIPTOR_OPERATION_WRITE = 0x02
EMBER_AF_FILE_DESCRIPTOR_OPERATION_EXCEPT = 0x03
EMBER_AF_FILE_DESCRIPTOR_OPERATION_MAX
}
Typedefs#
typedef void(*
EmberAfFileDescriptorReadyCallback)(void *data, EmberAfFileDescriptorOperation operation)
Functions#
void
Bad file descriptor.
API Documentation#
emberAfPluginFileDescriptorDispatchAdd#
EmberStatus emberAfPluginFileDescriptorDispatchAdd (EmberAfFileDescriptorDispatchStruct * dispatchStruct)
Parameters
N/A | dispatchStruct |
Definition at line
56
of file app/framework/plugin-host/file-descriptor-dispatch/file-descriptor-dispatch.h
emberAfPluginFileDescriptorDispatchWaitForEvents#
EmberStatus emberAfPluginFileDescriptorDispatchWaitForEvents (uint32_t timeoutMs)
Parameters
N/A | timeoutMs |
Definition at line
57
of file app/framework/plugin-host/file-descriptor-dispatch/file-descriptor-dispatch.h
emberAfPluginFileDescriptorDispatchRemove#
bool emberAfPluginFileDescriptorDispatchRemove (int fileDescriptor)
Parameters
N/A | fileDescriptor |
Definition at line
58
of file app/framework/plugin-host/file-descriptor-dispatch/file-descriptor-dispatch.h
Enumeration Documentation#
EmberAfFileDescriptorOperation#
EmberAfFileDescriptorOperation
Enumerator | |
---|---|
EMBER_AF_FILE_DESCRIPTOR_OPERATION_NONE | |
EMBER_AF_FILE_DESCRIPTOR_OPERATION_READ | |
EMBER_AF_FILE_DESCRIPTOR_OPERATION_WRITE | |
EMBER_AF_FILE_DESCRIPTOR_OPERATION_EXCEPT | |
EMBER_AF_FILE_DESCRIPTOR_OPERATION_MAX |
Definition at line
34
of file app/framework/plugin-host/file-descriptor-dispatch/file-descriptor-dispatch.h
Typedef Documentation#
EmberAfFileDescriptorReadyCallback#
typedef void(* EmberAfFileDescriptorReadyCallback) (void *data, EmberAfFileDescriptorOperation operation) )(void *data, EmberAfFileDescriptorOperation operation)
Definition at line
42
of file app/framework/plugin-host/file-descriptor-dispatch/file-descriptor-dispatch.h
Function Documentation#
emberAfPluginFileDescriptorDispatchBadFileDescriptorCallback#
void emberAfPluginFileDescriptorDispatchBadFileDescriptorCallback (int fd)
Bad file descriptor.
Parameters
N/A | fd | The bad file descriptor Ver.: always |
The indicated file descriptor has been detected to be bad. For example, the file descriptor caused an EBADF error on a select() call. The file descriptor will be omitted from subsequent file descriptor polling. The application responsible for the file descriptor should take steps to recover and clean up.
Definition at line
72
of file app/framework/plugin-host/file-descriptor-dispatch/file-descriptor-dispatch.h