Modules#

End Device Support

End Device Support#

API and Callbacks for the End Device Support Component.

Silicon Labs implementation of polling for end devices. Note that the Poll Control Server component sets the long and short poll intervals at startup. If both components are enabled, the long and short poll intervals set here will not be used.

Handlers Documentation#

emberAfPluginEndDeviceSupportMoveNetworkEventHandler#

void emberAfPluginEndDeviceSupportMoveNetworkEventHandler (SLXU_UC_EVENT )
Parameters
N/A

Definition at line 71 of file app/framework/plugin/end-device-support/end-device-support.h