DMP UI Demo Stub#
API and Callbacks for the DMP UI Demo Stub Component.
This component provides stubs for the DynamicMultiprotocolDemoLight app. Use this component to satisfy compilation when the display driver is not used, primarily when the Dynamic Multiprotocol UI Demo Code component is not enabled.
API#
enum
DMP_UI_LIGHT_ON
DMP_UI_LIGHT_OFF
DMP_UI_LIGHT_UNCHANGED
DMP_UI_LIGHT_OFF
DMP_UI_LIGHT_ON
DMP_UI_LIGHT_UNCHANGED
}
#define
#define
#define
sl_dmp_ui_light_off (void)
#define
sl_dmp_ui_light_on (void)
#define
#define
#define
#define
#define
sl_dmp_ui_display_help (void)
#define
#define
#define
#define
#define
DmpUiLightDirection_t uint8_t
#define
#define
API Documentation#
sl_dmp_ui_light_state_t#
sl_dmp_ui_light_state_t
Enumerator | |
---|---|
DMP_UI_LIGHT_ON | |
DMP_UI_LIGHT_OFF | |
DMP_UI_LIGHT_UNCHANGED | |
DMP_UI_LIGHT_OFF | |
DMP_UI_LIGHT_ON | |
DMP_UI_LIGHT_UNCHANGED |
Definition at line
61
of file app/framework/plugin/dmp-ui-demo-stub/dmp-ui-stub.h
sl_dmp_ui_display_zigbee_state#
#define sl_dmp_ui_display_zigbee_state
Definition at line
44
of file app/framework/plugin/dmp-ui-demo-stub/dmp-ui-stub.h
sl_dmp_ui_zigbee_permit_join#
#define sl_dmp_ui_zigbee_permit_join
Definition at line
45
of file app/framework/plugin/dmp-ui-demo-stub/dmp-ui-stub.h
sl_dmp_ui_light_off#
#define sl_dmp_ui_light_off
Definition at line
46
of file app/framework/plugin/dmp-ui-demo-stub/dmp-ui-stub.h
sl_dmp_ui_light_on#
#define sl_dmp_ui_light_on
Definition at line
47
of file app/framework/plugin/dmp-ui-demo-stub/dmp-ui-stub.h
sl_dmp_ui_update_direction#
#define sl_dmp_ui_update_direction
Definition at line
48
of file app/framework/plugin/dmp-ui-demo-stub/dmp-ui-stub.h
sl_dmp_ui_bluetooth_connected#
#define sl_dmp_ui_bluetooth_connected
Definition at line
49
of file app/framework/plugin/dmp-ui-demo-stub/dmp-ui-stub.h
sl_dmp_ui_set_ble_device_name#
#define sl_dmp_ui_set_ble_device_name
Definition at line
50
of file app/framework/plugin/dmp-ui-demo-stub/dmp-ui-stub.h
sl_dmp_ui_init#
#define sl_dmp_ui_init
Definition at line
51
of file app/framework/plugin/dmp-ui-demo-stub/dmp-ui-stub.h
sl_dmp_ui_display_help#
#define sl_dmp_ui_display_help
Definition at line
52
of file app/framework/plugin/dmp-ui-demo-stub/dmp-ui-stub.h
DMP_UI_DIRECTION_INVALID#
#define DMP_UI_DIRECTION_INVALIDValue:
0
Definition at line
53
of file app/framework/plugin/dmp-ui-demo-stub/dmp-ui-stub.h
DMP_UI_DIRECTION_BLUETOOTH#
#define DMP_UI_DIRECTION_BLUETOOTHValue:
1
Definition at line
54
of file app/framework/plugin/dmp-ui-demo-stub/dmp-ui-stub.h
DMP_UI_DIRECTION_SWITCH#
#define DMP_UI_DIRECTION_SWITCHValue:
2
Definition at line
55
of file app/framework/plugin/dmp-ui-demo-stub/dmp-ui-stub.h
DMP_UI_DIRECTION_ZIGBEE#
#define DMP_UI_DIRECTION_ZIGBEEValue:
3
Definition at line
56
of file app/framework/plugin/dmp-ui-demo-stub/dmp-ui-stub.h
DmpUiLightDirection_t#
#define DmpUiLightDirection_tValue:
uint8_t
Definition at line
57
of file app/framework/plugin/dmp-ui-demo-stub/dmp-ui-stub.h
sl_dmp_ui_set_light_direction#
#define sl_dmp_ui_set_light_direction
Definition at line
58
of file app/framework/plugin/dmp-ui-demo-stub/dmp-ui-stub.h
sl_dmp_ui_get_light_direction#
#define sl_dmp_ui_get_light_directionValue:
(...)
Definition at line
59
of file app/framework/plugin/dmp-ui-demo-stub/dmp-ui-stub.h