Modules#
MAC Address Filtering#
API and Callbacks for the MAC Address Filtering Component.
This plugin artificially limits what the stack hears by filtering the packets just above the lower MAC. The plugin can be configured on the fly via CLI with the short or long address of devices whose packets will be dropped or allowed. There are two lists, a short address list (2-byte node ID) and a long address list (8-byte IEEE address). Each list may be configured as either a whitelist or blacklist. The default is a blacklist with no addresses configured (accept all packets normally). A separate option allows or drops packets with no address information (e.g., Beacon Requests). NOTE: The radio will still generate and process MAC ACKs for packets. This plugin cannot be used to effect the behavior of MAC ACKs, which are handled by the RAIL library and radio hardware.
API#
Print configuration command.
filter out the no address command
add the short address command
set the short address list type
set the long address list type
Add long address.
Clear the short address list.
clear the long address list
Add panID.
Delete a panID entry.
Clear the panID list.
set list type for panID list
MAC address filtering reset.
Clear all lists for MAC address filtering.
Delete an entry from short address list.
Delete an entry from long address list.
Get stats for a short address.
Get MAC address filtering stats. Get the allowed, dropped and total packet counts.
API Documentation#
emberAfPluginMacAddressFilteringPrintConfigCommand#
void emberAfPluginMacAddressFilteringPrintConfigCommand (SL_CLI_COMMAND_ARG )
Print configuration command.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| SL_CLI_COMMAND_ARG | N/A | Ver.: always |
emberAfPluginMacAddressFilteringFilterNoAddressCommand#
void emberAfPluginMacAddressFilteringFilterNoAddressCommand (SL_CLI_COMMAND_ARG )
filter out the no address command
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| SL_CLI_COMMAND_ARG | N/A | Ver.: always |
emberAfPluginMacAddressFilteringAddShortAddressCommand#
void emberAfPluginMacAddressFilteringAddShortAddressCommand (SL_CLI_COMMAND_ARG )
add the short address command
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| SL_CLI_COMMAND_ARG | N/A | Ver.: always |
emberAfPluginMacAddressFilteringSetShortAddressListType#
void emberAfPluginMacAddressFilteringSetShortAddressListType (SL_CLI_COMMAND_ARG )
set the short address list type
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| SL_CLI_COMMAND_ARG | N/A | Ver.: always |
emberAfPluginMacAddressFilteringSetLongAddressListType#
void emberAfPluginMacAddressFilteringSetLongAddressListType (SL_CLI_COMMAND_ARG )
set the long address list type
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| SL_CLI_COMMAND_ARG | N/A | Ver.: always |
emberAfPluginMacAddressFilteringAddLongAddressCommand#
void emberAfPluginMacAddressFilteringAddLongAddressCommand (SL_CLI_COMMAND_ARG )
Add long address.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| SL_CLI_COMMAND_ARG | N/A | Ver.: always |
emberAfPluginMacAddressFilteringClearShortAddressList#
void emberAfPluginMacAddressFilteringClearShortAddressList (SL_CLI_COMMAND_ARG )
Clear the short address list.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| SL_CLI_COMMAND_ARG | N/A | Ver.: always |
emberAfPluginMacAddressFilteringClearLongAddressList#
void emberAfPluginMacAddressFilteringClearLongAddressList (SL_CLI_COMMAND_ARG )
clear the long address list
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| SL_CLI_COMMAND_ARG | N/A | Ver.: always |
emberAfPluginMacAddressFilteringAddPanIdCommand#
void emberAfPluginMacAddressFilteringAddPanIdCommand (SL_CLI_COMMAND_ARG )
Add panID.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| SL_CLI_COMMAND_ARG | N/A | Ver.: always |
emberAfPluginMacAddressFilteringPanIdDeleteEntry#
void emberAfPluginMacAddressFilteringPanIdDeleteEntry (SL_CLI_COMMAND_ARG )
Delete a panID entry.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| SL_CLI_COMMAND_ARG | N/A | Ver.: always |
emberAfPluginMacAddressFilteringClearPanIdList#
void emberAfPluginMacAddressFilteringClearPanIdList (SL_CLI_COMMAND_ARG )
Clear the panID list.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| SL_CLI_COMMAND_ARG | N/A | Ver.: always |
emberAfPluginMacAddressFilteringSetPanIdListType#
void emberAfPluginMacAddressFilteringSetPanIdListType (SL_CLI_COMMAND_ARG )
set list type for panID list
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| SL_CLI_COMMAND_ARG | N/A | Ver.: always |
emberAfPluginMacAddressFilteringReset#
void emberAfPluginMacAddressFilteringReset (SL_CLI_COMMAND_ARG )
MAC address filtering reset.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| SL_CLI_COMMAND_ARG | N/A | Ver.: always |
emberAfPluginMacAddressFilteringClearAll#
void emberAfPluginMacAddressFilteringClearAll (void )
Clear all lists for MAC address filtering.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A | Ver.: always |
emberAfPluginMacAddressFilteringShortAddressDeleteEntry#
void emberAfPluginMacAddressFilteringShortAddressDeleteEntry (SL_CLI_COMMAND_ARG )
Delete an entry from short address list.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| SL_CLI_COMMAND_ARG | N/A | Ver.: always |
emberAfPluginMacAddressFilteringLongAddressDeleteEntry#
void emberAfPluginMacAddressFilteringLongAddressDeleteEntry (SL_CLI_COMMAND_ARG )
Delete an entry from long address list.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| SL_CLI_COMMAND_ARG | N/A | Ver.: always |
emberAfPluginMacAddressFilteringGetStatsForShortAddress#
EmberStatus emberAfPluginMacAddressFilteringGetStatsForShortAddress (uint8_t index, uint32_t * matchCountForIndexPtr)
Get stats for a short address.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | N/A | index | Ver.: always |
| uint32_t * | N/A | matchCountForIndexPtr | Ver.: always |
Returns
EmberStatus status code
emberAfPluginMacAddressFilteringGetStats#
void emberAfPluginMacAddressFilteringGetStats (bool shortMode, uint32_t * allowedPacketCountPtr, uint32_t * droppedPacketCountPtr, uint32_t * totalPacketCountPtr)
Get MAC address filtering stats. Get the allowed, dropped and total packet counts.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| bool | N/A | shortMode | Ver.: always |
| uint32_t * | N/A | allowedPacketCountPtr | Ver.: always |
| uint32_t * | N/A | droppedPacketCountPtr | Ver.: always |
| uint32_t * | N/A | totalPacketCountPtr | Ver.: always |