Delayed Join#
API and Callbacks for the Delayed Join Component.
This component is used both for a trust center and a joining device. It provides a set of APIs for setting the acceptable delay for receiving a network key, as well as sending the network key on demand from the app. The following are the minimum conditions to verify before successfully using this component:
1.The trust center must have an acceptable version of a link key for the joining devices.
2.The component must be (re-)activated every time a network is opened or after any other event that changes the trust center (re-)join policy.
API#
void
emberAfPluginDelayedJoinSetNetworkKeyTimeout(uint8_t timeout)
Set the network timeout value.
Macros#
#define
EMBER_AF_PLUGIN_DELAYED_JOIN_PLUGIN_NAME "Delayed Join"
API Documentation#
emberAfPluginDelayedJoinSetNetworkKeyTimeout#
void emberAfPluginDelayedJoinSetNetworkKeyTimeout (uint8_t timeout)
Set the network timeout value.
Parameters
N/A | timeout | timeout value. Acceptable range 3-255 Ver.: always |
Definition at line
55
of file app/framework/plugin/delayed-join/delayed-join.h