Compact Logger#
Callbacks for Compact Logger Component.
Callbacks#
void
emberAfPluginCompactLoggerUtcTimeSetCallback(uint32_t currentUtcTimeSeconds)
Return the current UTC time.
Callbacks Documentation#
emberAfPluginCompactLoggerUtcTimeSetCallback#
void emberAfPluginCompactLoggerUtcTimeSetCallback (uint32_t currentUtcTimeSeconds)
Return the current UTC time.
Parameters
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint32_t | N/A | currentUtcTimeSeconds | The current UTC time in seconds. Ver.: always |
This function is called when the UTC time has been set. It returns the current UTC time. This callback is fired after all applicable compact-logger events have had their UTC time updated.