Contain the superset of values passed to both emberIncomingMessageHandler on the SoC and ezspIncomingMessageHandler on the host.
Public Attributes#
EmberIncomingMessageType
EmberApsFrame *
uint8_t *
uint16_t
uint16_t
uint8_t
int8_t
uint8_t
uint8_t
uint8_t
Public Attribute Documentation#
lastHopLqi#
uint8_t EmberAfIncomingMessage::lastHopLqi
Link quality from the node that last relayed the message.
lastHopRssi#
int8_t EmberAfIncomingMessage::lastHopRssi
The energy level (in units of dBm) observed during the reception.
bindingTableIndex#
uint8_t EmberAfIncomingMessage::bindingTableIndex
The index of a binding that matches the message or 0xFF if there is no matching binding.
addressTableIndex#
uint8_t EmberAfIncomingMessage::addressTableIndex
The index of the entry in the address table that matches the sender of the message or 0xFF if there is no matching entry.
networkIndex#
uint8_t EmberAfIncomingMessage::networkIndex
The index of the network on which this message was received.