This is a unique identifier for referencing Zigbee Over-the-air upgrade images. It is used by the OTA plugins when passing around information about an upgrade file.

Public Attributes#

uint16_t

Public Attribute Documentation#

manufacturerId#

uint16_t EmberAfOtaImageId::manufacturerId

imageTypeId#

uint16_t EmberAfOtaImageId::imageTypeId

firmwareVersion#

uint32_t EmberAfOtaImageId::firmwareVersion

deviceSpecificFileEui64#

uint8_t EmberAfOtaImageId::deviceSpecificFileEui64[EUI64_SIZE]

This is only used for device-specific files. It will be set to all zeroes when the image does not have an upgrade destination field in it. Little endian format.