Describe clusters that are on the endpoint.
Public Attribute Documentation#
cluster#
EmberAfCluster* EmberAfEndpointType::cluster
Pointer to the cluster structs, describing clusters on this endpoint type.
Definition at line
454
of file app/framework/include/af-types.h
clusterCount#
uint8_t EmberAfEndpointType::clusterCount
Number of clusters in this endpoint type.
Definition at line
458
of file app/framework/include/af-types.h
endpointSize#
uint16_t EmberAfEndpointType::endpointSize
Size of all non-external, non-singlet attribute, in this endpoint type.
Definition at line
462
of file app/framework/include/af-types.h