Keep track of cluster-related events and their sleep control values. The cluster code will not know at runtime all of the events that it has access to in the event table This structure is stored by the application framework in an event context table which along with helper functions allows the cluster code to schedule and deactivate its associated events.
Public Attribute Documentation#
endpoint#
uint8_t sl_zigbee_event_context_t::endpoint
The endpoint of the associated cluster event.
861
of file app/framework/include/af-types.h
clusterId#
EmberAfClusterId sl_zigbee_event_context_t::clusterId
The cluster ID of the associated cluster event.
865
of file app/framework/include/af-types.h
isClient#
bool sl_zigbee_event_context_t::isClient
The server/client identity of the associated cluster event.
869
of file app/framework/include/af-types.h
pollControl#
EmberAfEventPollControl sl_zigbee_event_context_t::pollControl
A poll control value used to control the network polling behavior while the event is active.
874
of file app/framework/include/af-types.h
sleepControl#
EmberAfEventSleepControl sl_zigbee_event_context_t::sleepControl
A sleep control value used to control the processor's sleep behavior while the event is active.
879
of file app/framework/include/af-types.h
event#
sl_zigbee_event_t* sl_zigbee_event_context_t::event
A pointer to the event control value which is stored in the event table and is used to actually schedule the event.
884
of file app/framework/include/af-types.h