Store scene table entries in RAM or in tokens, depending on a plugin setting. If endpoint field is EMBER_AF_SCENE_TABLE_UNUSED_ENDPOINT_ID, the entry is unused.

Public Attributes#

uint8_t
uint16_t
uint8_t

Public Attribute Documentation#

endpoint#

uint8_t EmberAfSceneTableEntry::endpoint

Definition at line 960 of file app/framework/include/af-types.h

groupId#

uint16_t EmberAfSceneTableEntry::groupId

Definition at line 961 of file app/framework/include/af-types.h

sceneId#

uint8_t EmberAfSceneTableEntry::sceneId

Definition at line 962 of file app/framework/include/af-types.h

transitionTime#

uint16_t EmberAfSceneTableEntry::transitionTime

Definition at line 966 of file app/framework/include/af-types.h

transitionTime100ms#

uint8_t EmberAfSceneTableEntry::transitionTime100ms

Definition at line 967 of file app/framework/include/af-types.h