Describe a load control event.
This struct is used in the load control event callback and within the demand response load control cluster code.
Public Attributes#
uint32_t
uint8_t
uint16_t
uint8_t
uint32_t
uint16_t
uint8_t
uint8_t
uint8_t
int16_t
int16_t
int8_t
uint8_t
uint8_t
uint32_t
uint32_t
uint8_t
Public Attribute Documentation#
eventId#
uint32_t EmberAfLoadControlEvent::eventId
Definition at line
584
of file app/framework/include/af-types.h
destinationEndpoint#
uint8_t EmberAfLoadControlEvent::destinationEndpoint
Definition at line
594
of file app/framework/include/af-types.h
deviceClass#
uint16_t EmberAfLoadControlEvent::deviceClass
Definition at line
595
of file app/framework/include/af-types.h
utilityEnrollmentGroup#
uint8_t EmberAfLoadControlEvent::utilityEnrollmentGroup
Definition at line
596
of file app/framework/include/af-types.h
startTime#
uint32_t EmberAfLoadControlEvent::startTime
Start time in seconds
Definition at line
600
of file app/framework/include/af-types.h
duration#
uint16_t EmberAfLoadControlEvent::duration
Duration in minutes
Definition at line
604
of file app/framework/include/af-types.h
criticalityLevel#
uint8_t EmberAfLoadControlEvent::criticalityLevel
Definition at line
605
of file app/framework/include/af-types.h
coolingTempOffset#
uint8_t EmberAfLoadControlEvent::coolingTempOffset
Definition at line
606
of file app/framework/include/af-types.h
heatingTempOffset#
uint8_t EmberAfLoadControlEvent::heatingTempOffset
Definition at line
607
of file app/framework/include/af-types.h
coolingTempSetPoint#
int16_t EmberAfLoadControlEvent::coolingTempSetPoint
Definition at line
608
of file app/framework/include/af-types.h
heatingTempSetPoint#
int16_t EmberAfLoadControlEvent::heatingTempSetPoint
Definition at line
609
of file app/framework/include/af-types.h
avgLoadPercentage#
int8_t EmberAfLoadControlEvent::avgLoadPercentage
Definition at line
610
of file app/framework/include/af-types.h
dutyCycle#
uint8_t EmberAfLoadControlEvent::dutyCycle
Definition at line
611
of file app/framework/include/af-types.h
eventControl#
uint8_t EmberAfLoadControlEvent::eventControl
Definition at line
612
of file app/framework/include/af-types.h
startRand#
uint32_t EmberAfLoadControlEvent::startRand
Definition at line
613
of file app/framework/include/af-types.h
durationRand#
uint32_t EmberAfLoadControlEvent::durationRand
Definition at line
614
of file app/framework/include/af-types.h
optionControl#
uint8_t EmberAfLoadControlEvent::optionControl
Definition at line
615
of file app/framework/include/af-types.h