Contain the superset of values passed to both emberIncomingMessageHandler on the SoC and ezspIncomingMessageHandler on the host.

Public Attributes#

EmberIncomingMessageType
EmberApsFrame *
uint8_t *
uint16_t
uint16_t
uint8_t

Public Attribute Documentation#

type#

EmberIncomingMessageType EmberAfIncomingMessage::type

The type of the incoming message.


Definition at line 299 of file app/framework/include/af-types.h

apsFrame#

EmberApsFrame* EmberAfIncomingMessage::apsFrame

APS frame for the incoming message.


Definition at line 303 of file app/framework/include/af-types.h

message#

uint8_t* EmberAfIncomingMessage::message

The message copied into a flat buffer.


Definition at line 307 of file app/framework/include/af-types.h

msgLen#

uint16_t EmberAfIncomingMessage::msgLen

Length of the incoming message.


Definition at line 311 of file app/framework/include/af-types.h

source#

uint16_t EmberAfIncomingMessage::source

Two byte node ID of the sending node.


Definition at line 315 of file app/framework/include/af-types.h

lastHopLqi#

uint8_t EmberAfIncomingMessage::lastHopLqi

Link quality from the node that last relayed the message.


Definition at line 320 of file app/framework/include/af-types.h

lastHopRssi#

int8_t EmberAfIncomingMessage::lastHopRssi

The energy level (in units of dBm) observed during the reception.


Definition at line 324 of file app/framework/include/af-types.h

bindingTableIndex#

uint8_t EmberAfIncomingMessage::bindingTableIndex

The index of a binding that matches the message or 0xFF if there is no matching binding.


Definition at line 329 of file app/framework/include/af-types.h

addressTableIndex#

uint8_t EmberAfIncomingMessage::addressTableIndex

The index of the entry in the address table that matches the sender of the message or 0xFF if there is no matching entry.


Definition at line 335 of file app/framework/include/af-types.h

networkIndex#

uint8_t EmberAfIncomingMessage::networkIndex

The index of the network on which this message was received.


Definition at line 339 of file app/framework/include/af-types.h