Contain basic information about an endpoint.

Public Attribute Documentation#

clusters#

EmberAfClusterInfo EmberAfEndpointInfoStruct::clusters[EMBER_AF_MAX_CLUSTERS_PER_ENDPOINT]

Definition at line 1906 of file app/framework/include/af-types.h

profileId#

EmberAfProfileId EmberAfEndpointInfoStruct::profileId

Definition at line 1907 of file app/framework/include/af-types.h

deviceId#

uint16_t EmberAfEndpointInfoStruct::deviceId

Definition at line 1908 of file app/framework/include/af-types.h

endpoint#

uint8_t EmberAfEndpointInfoStruct::endpoint

Definition at line 1909 of file app/framework/include/af-types.h

clusterCount#

uint8_t EmberAfEndpointInfoStruct::clusterCount

Definition at line 1910 of file app/framework/include/af-types.h