Passed to the emberAfImageBlockRequestCallback() to let the application decide what to do.
Public Attributes#
const EmberAfOtaImageId *
uint32_t
uint32_t
EmberNodeId
EmberEUI64
uint16_t
uint8_t
uint8_t
Public Attribute Documentation#
id#
const EmberAfOtaImageId* EmberAfImageBlockRequestCallbackStruct::id
Definition at line
1239
of file app/framework/include/af-types.h
offset#
uint32_t EmberAfImageBlockRequestCallbackStruct::offset
Definition at line
1240
of file app/framework/include/af-types.h
waitTimeSecondsResponse#
uint32_t EmberAfImageBlockRequestCallbackStruct::waitTimeSecondsResponse
Definition at line
1241
of file app/framework/include/af-types.h
source#
EmberNodeId EmberAfImageBlockRequestCallbackStruct::source
Definition at line
1242
of file app/framework/include/af-types.h
sourceEui#
EmberEUI64 EmberAfImageBlockRequestCallbackStruct::sourceEui
Definition at line
1243
of file app/framework/include/af-types.h
minBlockRequestPeriod#
uint16_t EmberAfImageBlockRequestCallbackStruct::minBlockRequestPeriod
Definition at line
1247
of file app/framework/include/af-types.h
maxDataSize#
uint8_t EmberAfImageBlockRequestCallbackStruct::maxDataSize
Definition at line
1248
of file app/framework/include/af-types.h
clientEndpoint#
uint8_t EmberAfImageBlockRequestCallbackStruct::clientEndpoint
Definition at line
1249
of file app/framework/include/af-types.h
bitmask#
EmberAfImageBlockRequestOptions EmberAfImageBlockRequestCallbackStruct::bitmask
Definition at line
1250
of file app/framework/include/af-types.h