Green Power Client#
Callbacks for Green Power Client Component.
Callbacks#
void
emberAfGreenPowerClientGpdfSinkTableBasedForwardCallback(EmberGpAddress *addr, EmberGpSinkListEntry *sinkList, uint8_t maxNumberEntries)
Green power client Sink table based forward callback.
Callbacks Documentation#
emberAfGreenPowerClientGpdfSinkTableBasedForwardCallback#
void emberAfGreenPowerClientGpdfSinkTableBasedForwardCallback (EmberGpAddress * addr, EmberGpSinkListEntry * sinkList, uint8_t maxNumberEntries)
Green power client Sink table based forward callback.
Parameters
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| EmberGpAddress * | N/A | addr | gpd address Ver.: always |
| EmberGpSinkListEntry * | N/A | sinkList | sink list pointer , that can be used to update the sink list Ver.: always |
| uint8_t | N/A | maxNumberEntries | maximum number of sink list entires Ver.: always |
This function is called by the Green Power client before forwarding the gp notification. This callback provides the pointer to the group list for the paired gpd. In case of a combo application, where the green power server is also present, this callback is consumed by the green power server to update the sinklist from the sink table.