WWAH Client Silicon Labs#
Callbacks for WWAH Client Silicon Labs Component.
Callbacks#
void
emberAfSlWwahClusterClientInitCallback(uint8_t endpoint)
WWAH cluster client init callback.
bool
emberAfSlWwahClusterDebugReportQueryResponseCallback(uint8_t debugReportId, uint8_t *debugReportData)
WWAH cluster debug report query response callback.
Callbacks Documentation#
emberAfSlWwahClusterClientInitCallback#
void emberAfSlWwahClusterClientInitCallback (uint8_t endpoint)
WWAH cluster client init callback.
Parameters
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | N/A | endpoint | end point |
emberAfSlWwahClusterDebugReportQueryResponseCallback#
bool emberAfSlWwahClusterDebugReportQueryResponseCallback (uint8_t debugReportId, uint8_t * debugReportData)
WWAH cluster debug report query response callback.
Parameters
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | N/A | debugReportId | debug report ID |
| uint8_t * | N/A | debugReportData | debug report data |