GP Client Commissioning State.

Public Attribute Documentation#

inCommissioningMode#

bool sl_zigbee_af_green_power_client_commissioning_state_t::inCommissioningMode

If GP Client is in Commissioning Mode


exitMode#

sl_zigbee_af_green_power_client_commissioning_exit_mode_t sl_zigbee_af_green_power_client_commissioning_state_t::exitMode

GP Client Commissioning Mode exit flag


gppCommissioningWindow#

uint16_t sl_zigbee_af_green_power_client_commissioning_state_t::gppCommissioningWindow

GP Proxy Commissioning Window


channel#

uint8_t sl_zigbee_af_green_power_client_commissioning_state_t::channel

GP Client current channel


unicastCommunication#

bool sl_zigbee_af_green_power_client_commissioning_state_t::unicastCommunication

If Commissioning is unicast or broadcast


commissioningSink#

sl_802154_short_addr_t sl_zigbee_af_green_power_client_commissioning_state_t::commissioningSink

Address of GP Commissioning Sink


channelStatus#

uint8_t sl_zigbee_af_green_power_client_commissioning_state_t::channelStatus

GP Client status flags. Bit 0 shows if we are on transmit channel(1) or on operational channel(0). bit 1 shows if operational channel is same as transmit channel (1)