Address Table#

API and Callbacks for the Address Table Component.

This component supports managing the address table. On the SoC, all actions are directly performed on the stack address table. The host maintains a copy of the address table and ensures that it is always in sync with the NCP's address table. When building the Host, make sure that the NCP can support the address table size in the component configuration. The optimal size varies based on the platform architecture and size of other dynamically-allocated data for this application. If errors occur upon reseting the NCP, the NCP may not have enough room to store a large address table size. If this is not the case, the NCP may not be able to dynamically increase the address table size based on the host's request. To work around this issue, statically allocate the desired address table size on the Zigbee Pro Stack\Pro Leaf Stack components on the NCP.

API#

sl_status_t
sl_zigbee_af_address_table_remove_entry(sl_802154_long_addr_t entry)

Remove an entry from the address table.

uint8_t

Add a new entry to the address table.

sl_status_t
sl_zigbee_af_address_table_lookup_by_index(uint8_t index, sl_802154_long_addr_t entry)

Copy the entry stored at the passed index to the passed variable and return SL_STATUS_OK if the passed index is valid.

sl_802154_short_addr_t

Copy the entry stored at the passed index to the passed variable and return SL_STATUS_OK if the passed index is valid.

sl_status_t
sl_zigbee_af_send_unicast_to_eui64(sl_802154_long_addr_t destination, sl_zigbee_aps_frame_t *apsFrame, uint16_t messageLength, uint8_t *message)

Allow sending a unicast message specifying the EUI64 of the destination node.

sl_status_t
sl_zigbee_af_send_command_unicast_to_eui64(sl_802154_long_addr_t destination)

Send the command prepared with sl_zigbee_af_fill.... macro.

sl_status_t
sl_zigbee_af_get_current_sender_eui64(sl_802154_long_addr_t address)

Copy the sender EUI64, if available, to the address parameter and return SL_STATUS_OK. Otherwise, return SL_STATUS_INVALID_STATE.

#define
sl_zigbee_af_address_table_add_entry (longId)

Add a new entry to the address table.

#define
sl_zigbee_af_address_table_remove_entry_by_index (index)

Remove an entry from the address table by index.

#define
sl_zigbee_af_address_table_lookup_by_eui64 (longId)

Search for an EUI64 in the address table.

API Documentation#

sl_zigbee_af_address_table_remove_entry#

sl_status_t sl_zigbee_af_address_table_remove_entry (sl_802154_long_addr_t entry)

Remove an entry from the address table.

Parameters
TypeDirectionArgument NameDescription
sl_802154_long_addr_tN/Aentry

If the entry exists, the entry is cleared and the SL_STATUS_OK status is returned. Otherwise, the status SL_STATUS_INVALID_STATE is returned.


sl_zigbee_af_lookup_address_table_entry_by_eui64#

uint8_t sl_zigbee_af_lookup_address_table_entry_by_eui64 (sl_802154_long_addr_t longId)

Add a new entry to the address table.

Parameters
TypeDirectionArgument NameDescription
sl_802154_long_addr_tN/AlongId

If the entry already exists, no new entry is created and the index of the entry already in the table is returned. If a free entry is found, the entry is added to the table and the corresponding index is returned. If no free entry is available in the address table, the value SL_ZIGBEE_NULL_ADDRESS_TABLE_INDEX is returned.


sl_zigbee_af_address_table_lookup_by_index#

sl_status_t sl_zigbee_af_address_table_lookup_by_index (uint8_t index, sl_802154_long_addr_t entry)

Copy the entry stored at the passed index to the passed variable and return SL_STATUS_OK if the passed index is valid.

Parameters
TypeDirectionArgument NameDescription
uint8_tN/Aindex
sl_802154_long_addr_tN/Aentry

Otherwise, the status SL_STATUS_INVALID_STATE is returned.


sl_zigbee_af_address_table_lookup_node_id_by_index#

sl_802154_short_addr_t sl_zigbee_af_address_table_lookup_node_id_by_index (uint8_t index)

Copy the entry stored at the passed index to the passed variable and return SL_STATUS_OK if the passed index is valid.

Parameters
TypeDirectionArgument NameDescription
uint8_tN/Aindex

Otherwise, the status SL_STATUS_INVALID_STATE is returned.


sl_zigbee_af_send_unicast_to_eui64#

sl_status_t sl_zigbee_af_send_unicast_to_eui64 (sl_802154_long_addr_t destination, sl_zigbee_aps_frame_t * apsFrame, uint16_t messageLength, uint8_t * message)

Allow sending a unicast message specifying the EUI64 of the destination node.

Parameters
TypeDirectionArgument NameDescription
sl_802154_long_addr_tN/Adestination
sl_zigbee_aps_frame_t *N/AapsFrame
uint16_tN/AmessageLength
uint8_t *N/Amessage

Note: the specified EUI64 must be present in the address table. Otherwise, the status SL_STATUS_INVALID_STATE is returned.


sl_zigbee_af_send_command_unicast_to_eui64#

sl_status_t sl_zigbee_af_send_command_unicast_to_eui64 (sl_802154_long_addr_t destination)

Send the command prepared with sl_zigbee_af_fill.... macro.

Parameters
TypeDirectionArgument NameDescription
sl_802154_long_addr_tN/Adestination

This function sends a command that was previously prepared using the sl_zigbee_af_fill... macros from the client command API. It will be sent as unicast to the node that corresponds in the address table to the passed EUI64.


sl_zigbee_af_get_current_sender_eui64#

sl_status_t sl_zigbee_af_get_current_sender_eui64 (sl_802154_long_addr_t address)

Copy the sender EUI64, if available, to the address parameter and return SL_STATUS_OK. Otherwise, return SL_STATUS_INVALID_STATE.

Parameters
TypeDirectionArgument NameDescription
sl_802154_long_addr_tN/Aaddress