Reporting#

API and Callbacks for the Reporting Component.

Silicon Labs implementation of reporting. Reports are asynchronous messages sent out when an ZCL attribute has changed. This component supports both requesting reports from another device and sending out attribute reports when the device has been configured to do so. If the application receives reports from multiple sources, Silicon Labs recommends configuring it as a concentrator. Note: This component only supports the binding-based interpretation of reporting in which reports are sent to corresponding entries in the binding table. Either the node sending the reports, the node receiving the reports, or another third-party configuration device may create the binding table entry(s) on the reporting node. For more details, refer to the Application Framework Developers Guide for the current SDK version.

Modules#

sli_zigbee_af_report_volatile_data_type

Reporting

API#

sl_zigbee_af_reporting_configure_reported_attribute(const sl_zigbee_af_plugin_reporting_entry_t *newEntry)

Configure the new reported attribute.

void

Load the default reporting configuration.

bool
sl_zigbee_af_reporting_get_reporting_config_defaults(sl_zigbee_af_plugin_reporting_entry_t *defaultConfiguration)

Get the default reporting configuration.

Macros#

#define
NULL_INDEX 0xFFFF
#define
CTM_REPORTING_TABLE SL_TOKEN_GET_DYNAMIC_TOKEN((SL_TOKEN_NVM3_REGION_ZIGBEE | 0x4000), 0)
#define
REPORTING_TABLE_MAX_RANGE 127
#define
REPORTING_TABLE_PLUGIN_SIZE (SL_ZIGBEE_AF_PLUGIN_REPORTING_TABLE_SIZE)
#define
REPORT_TABLE_SIZE (REPORTING_TABLE_PLUGIN_SIZE)

API Documentation#

sl_zigbee_af_reporting_configure_reported_attribute#

sl_zigbee_af_status_t sl_zigbee_af_reporting_configure_reported_attribute (const sl_zigbee_af_plugin_reporting_entry_t * newEntry)

Configure the new reported attribute.

Parameters
TypeDirectionArgument NameDescription
const sl_zigbee_af_plugin_reporting_entry_t *N/AnewEntry

Pointer to the struct containing the reporting configuration entry

Returns

  • sl_zigbee_af_status_t Status code


sl_zigbee_af_reporting_load_reporting_config_defaults#

void sl_zigbee_af_reporting_load_reporting_config_defaults (void )

Load the default reporting configuration.

Parameters
TypeDirectionArgument NameDescription
voidN/A

sl_zigbee_af_reporting_get_reporting_config_defaults#

bool sl_zigbee_af_reporting_get_reporting_config_defaults (sl_zigbee_af_plugin_reporting_entry_t * defaultConfiguration)

Get the default reporting configuration.

Parameters
TypeDirectionArgument NameDescription
sl_zigbee_af_plugin_reporting_entry_t *N/AdefaultConfiguration

Pointer to the struct where default configuration will be stored

Returns

  • bool true if there is a default value


Variable Documentation#

sli_zigbee_af_report_volatile_data#

sli_zigbee_af_report_volatile_data_type sli_zigbee_af_report_volatile_data[]