XModem Sender#
API and Callbacks for the XModem Sender Component.
API#
void
sl_zigbee_af_xmodem_sender_incoming_block(uint8_t *data, uint8_t length)
sl_status_t
sl_zigbee_af_xmodem_sender_start(sl_zigbee_af_xmodem_sender_transmit_function_t *sendRoutine, sl_zigbee_af_xmodem_sender_get_next_block_function_t *getNextBlockRoutine, sl_zigbee_af_xmodem_sender_finished_function_t *finishedRoutine, uint8_t maxSizeOfBlock, bool waitForReady)
void
Typedefs#
typedef sl_status_t()
sl_zigbee_af_xmodem_sender_transmit_function_t(uint8_t *data, uint8_t length)
typedef sl_status_t()
sl_zigbee_af_xmodem_sender_get_next_block_function_t(uint32_t address, uint8_t length, uint8_t *returnData, uint8_t *returnLength, bool *done)
typedef void()
sl_zigbee_af_xmodem_sender_finished_function_t(bool success)
Macros#
#define
XMODEM_SOH (0x01)
#define
XMODEM_EOT (0x04)
#define
XMODEM_ACK (0x06)
#define
XMODEM_NAK (0x15)
#define
XMODEM_CANCEL (0x18)
#define
XMODEM_BLOCKOK (0x19)
#define
XMODEM_FILEDONE (0x17)
API Documentation#
sl_zigbee_af_xmodem_sender_incoming_block#
void sl_zigbee_af_xmodem_sender_incoming_block (uint8_t * data, uint8_t length)
Parameters
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t * | N/A | data | |
| uint8_t | N/A | length |
sl_zigbee_af_xmodem_sender_start#
sl_status_t sl_zigbee_af_xmodem_sender_start (sl_zigbee_af_xmodem_sender_transmit_function_t * sendRoutine, sl_zigbee_af_xmodem_sender_get_next_block_function_t * getNextBlockRoutine, sl_zigbee_af_xmodem_sender_finished_function_t * finishedRoutine, uint8_t maxSizeOfBlock, bool waitForReady)
Parameters
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_zigbee_af_xmodem_sender_transmit_function_t * | N/A | sendRoutine | |
| sl_zigbee_af_xmodem_sender_get_next_block_function_t * | N/A | getNextBlockRoutine | |
| sl_zigbee_af_xmodem_sender_finished_function_t * | N/A | finishedRoutine | |
| uint8_t | N/A | maxSizeOfBlock | |
| bool | N/A | waitForReady |
sl_zigbee_af_xmodem_sender_abort#
void sl_zigbee_af_xmodem_sender_abort (void )
Parameters
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Typedef Documentation#
sl_zigbee_af_xmodem_sender_transmit_function_t#
typedef sl_status_t() sl_zigbee_af_xmodem_sender_transmit_function_t(uint8_t *data, uint8_t length) (uint8_t *data, uint8_t length)
sl_zigbee_af_xmodem_sender_get_next_block_function_t#
typedef sl_status_t() sl_zigbee_af_xmodem_sender_get_next_block_function_t(uint32_t address, uint8_t length, uint8_t *returnData, uint8_t *returnLength, bool *done) (uint32_t address, uint8_t length, uint8_t *returnData, uint8_t *returnLength, bool *done)
sl_zigbee_af_xmodem_sender_finished_function_t#
typedef void() sl_zigbee_af_xmodem_sender_finished_function_t(bool success) (bool success)