Network Creator#

API and Callbacks for the Network Creator Component.

This component performs the necessary steps to create a network according to the Base Device Behavior specification. The component performs an active scan followed by an energy scan across a primary channel set to decide which channel(s) are valid candidates for network formation. If the component fails to form a network on any primary channels, it moves to a secondary channel mask. Before every attempt at network formation, this component sets up the stack to use Zigbee 3.0 security.

Modules#

Network Creator

API#

sl_status_t
sl_zigbee_af_network_creator_start(bool centralizedNetwork)

Command the network creator to form a network with arbitrary PAN ID, TX power, and channel.

void

Stop the network creator process.

sl_status_t
sl_zigbee_af_network_creator_network_form(bool centralizedNetwork, sl_802154_pan_id_t panId, int8_t radioTxPower, uint8_t channel)

Command the network creator to form a network with the given qualities (arguments).

Variables#

uint32_t

The first set of channels that the plugin will scan when forming (hex) <0-0xFFFFFFFF> <f.h>

uint32_t

The second set of channels that the plugin will scan when forming (hex) <0-0xFFFFFFFF> <f.h>

Macros#

#define
SL_ZIGBEE_AF_PLUGIN_NETWORK_CREATOR_PLUGIN_NAME "NWK Creator"

API Documentation#

sl_zigbee_af_network_creator_start#

sl_status_t sl_zigbee_af_network_creator_start (bool centralizedNetwork)

Command the network creator to form a network with arbitrary PAN ID, TX power, and channel.

Parameters
TypeDirectionArgument NameDescription
bool[in]centralizedNetwork

Whether or not to form a network using centralized security. If this argument is false, a network with distributed security will be formed.

Returns

  • sl_status_t value that indicates either the successful formation of the new network, or the reason that the network formation failed.

    • ::SL_STATUS_INVALID_STATE if there is an ongoing scan or a network is already active.

    • ::SL_STATUS_FAIL if the scan queue is full.

    • ::SL_STATUS_OK if the network creator process has started.


sl_zigbee_af_network_creator_stop#

void sl_zigbee_af_network_creator_stop (void )

Stop the network creator process.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Stops the network creator formation process.


sl_zigbee_af_network_creator_network_form#

sl_status_t sl_zigbee_af_network_creator_network_form (bool centralizedNetwork, sl_802154_pan_id_t panId, int8_t radioTxPower, uint8_t channel)

Command the network creator to form a network with the given qualities (arguments).

Parameters
TypeDirectionArgument NameDescription
bool[in]centralizedNetwork

Indicates whether or not to form a network using centralized security. If this argument is false, a network with distributed security will be formed.

sl_802154_pan_id_t[in]panId

The pan ID of the network to be formed.

int8_t[in]radioTxPower

The TX power of the network to be formed.

uint8_t[in]channel

The channel of the network to be formed.

Commands the network creator to form a centralized or distributed network with specified PAN ID, TX power, and channel.

Returns

  • sl_status_t value that indicates either the successful formation of the new network, or the reason that the network formation failed.

    • ::SL_STATUS_INVALID_STATE if there is an ongoing scan or a network is already active.

    • ::SL_STATUS_FAIL if the scan queue is full.

    • ::SL_STATUS_OK if the network creator process has started.


Variable Documentation#

sli_zigbee_af_network_creator_primary_channel_mask#

uint32_t sli_zigbee_af_network_creator_primary_channel_mask

The first set of channels that the plugin will scan when forming (hex) <0-0xFFFFFFFF> <f.h>


sli_zigbee_af_network_creator_secondary_channel_mask#

uint32_t sli_zigbee_af_network_creator_secondary_channel_mask

The second set of channels that the plugin will scan when forming (hex) <0-0xFFFFFFFF> <f.h>