Gas Proxy Function#

API and Callbacks for the Gas Proxy Function Component.

Silicon Labs implementation of the Gas Proxy Function (GPF). This component receives and processes GBZ Top Off Messages. NOTE: This component uses malloc and should only be used in a non-SoC setup.

Modules#

Gas Proxy Function

Handlers#

sl_status_t
sl_zigbee_af_gas_proxy_function_non_tap_off_message_handler(uint8_t *gbzCommands, uint16_t gbzCommandsLength, uint16_t messageCode)
sl_status_t
sl_zigbee_af_gas_proxy_function_tap_off_message_handler(uint8_t *gbzCommand, uint16_t gbzCommandLength, uint8_t *gbzCommandResponse, uint16_t gbzCommandResponseLength, uint16_t messageCode)

API#

bool

Ignore future commands. Per GBCS v0.8.1, section 10.3.4.2 Step 12/13, it is inferred that per elemental ZCL command, future commands ( startTime greater than now ) will be discarded and the application will be notified.

Handlers Documentation#

sl_zigbee_af_gas_proxy_function_non_tap_off_message_handler#

sl_status_t sl_zigbee_af_gas_proxy_function_non_tap_off_message_handler (uint8_t * gbzCommands, uint16_t gbzCommandsLength, uint16_t messageCode)
Parameters
TypeDirectionArgument NameDescription
uint8_t *N/AgbzCommands
uint16_tN/AgbzCommandsLength
uint16_tN/AmessageCode

sl_zigbee_af_gas_proxy_function_tap_off_message_handler#

sl_status_t sl_zigbee_af_gas_proxy_function_tap_off_message_handler (uint8_t * gbzCommand, uint16_t gbzCommandLength, uint8_t * gbzCommandResponse, uint16_t gbzCommandResponseLength, uint16_t messageCode)
Parameters
TypeDirectionArgument NameDescription
uint8_t *N/AgbzCommand
uint16_tN/AgbzCommandLength
uint8_t *N/AgbzCommandResponse
uint16_tN/AgbzCommandResponseLength
uint16_tN/AmessageCode

API Documentation#

sl_zigbee_af_gas_proxy_function_ignore_future_command#

bool sl_zigbee_af_gas_proxy_function_ignore_future_command (uint32_t startTime)

Ignore future commands. Per GBCS v0.8.1, section 10.3.4.2 Step 12/13, it is inferred that per elemental ZCL command, future commands ( startTime greater than now ) will be discarded and the application will be notified.

Parameters
TypeDirectionArgument NameDescription
uint32_tN/AstartTime

Returns

  • true - if future dated current command are ignored, false - otherwise.