ZLL Commissioning Network#

API and Callbacks for the ZLL Commissioning Network Component.

(NOTE: This component is deprecated as it is not compliant to Zigbee 3.0 requirements. See Network Creator and Network Steering components instead for Zigbee 3.0-compliant implementations of this behavior.) Provides legacy Zigbee Light Link 1.0 implementation of routines for finding and joining any viable network via scanning, rather than joining a specific network.

Modules#

ZLL Commissioning Callback Network

API#

sl_status_t

Scan for joinable networks.

sl_status_t

Scan for an unused PAN ID.

API Documentation#

sl_zigbee_af_zll_scan_for_joinable_network#

sl_status_t sl_zigbee_af_zll_scan_for_joinable_network (void )

Scan for joinable networks.

Parameters
TypeDirectionArgument NameDescription
voidN/A

This function scans the primary channel set for joinable networks. If a joinable network is found, the plugin will attempt to join to it. If no joinable networks are found or if joining is not successful, the plugin will scan the secondary channel set for joinable networks. If a joinable network is found, the plugin will attempt to join to it. The plugin will only scan the secondary channel set if ::SL_ZIGBEE_AF_PLUGIN_ZLL_COMMISSIONING_COMMON_SCAN_SECONDARY_CHANNELS is defined. Otherwise, scanning stops after the initial scan of the primary channel set.

Routers and end devices should scan for joinable networks when directed by the application. Scanning for joinable networks enables classic Zigbee commissioning with non-ZLL devices.

Note, for Zigbee 3.0 compatibility, an application should use sl_zigbee_af_network_steering_start rather than this routine, which may be deprecated in a future release.

Returns

  • An ::sl_status_t value that indicates the success or failure of the command.


sl_zigbee_af_zll_scan_for_unused_pan_id#

sl_status_t sl_zigbee_af_zll_scan_for_unused_pan_id (void )

Scan for an unused PAN ID.

Parameters
TypeDirectionArgument NameDescription
voidN/A

This function scans the primary channel set for a channel with low average energy and then selects a PAN ID that is not in use on that channel. The plugin will then form a ZLL network on that channel with the chosen PAN ID.

Factory new routers may form a new ZLL network at startup, but this is not mandatory, since a network is created during touch linking if required. Similarly, a router may chose to form a new ZLL network if classical ZigBee commissioning has failed, but this is not mandatory either. However, if a router choses not to form a network, the application should call ::emberAfPluginZllCommissioningInitCallback to ensure the radio is switched on and is tuned to the default channel. Alternatively, the 'Rx always on' plugin option, ::EMBER_AF_PLUGIN_ZLL_COMMISSIONING_RX_ALWAYS_ON, may be set to true.

End devices should not use this API and should instead form ZLL networks via touch linking (or to be precise, join a ZLL network formed by a router target or a router initiator).

Note, for Zigbee 3.0 compatibility, a router device should use sl_zigbee_af_network_creator_start with centralizedNetwork=false to form a distributed network rather than this routine, which may be deprecated in a future release.

Returns

  • An ::sl_status_t value that indicates the success or failure of the command.