Sub GHz Client#

API and Callbacks for the Sub GHz Cluster Client Component.

The Smart Energy Sub-GHz client suspends the transmission of any ZCL messages for a given period when instructed so by the Sub-GHz server.

Modules#

Sub GHz Client

API#

sl_status_t
sl_zigbee_af_sub_ghz_client_send_get_suspend_zcl_messages_status_command(sl_802154_short_addr_t nodeId, uint8_t endpoint)

Send the 'Get Suspend ZCL Messages Status' command.

sl_status_t
sl_zigbee_af_sub_ghz_client_send_unsolicited_enhanced_update_notify(sl_802154_short_addr_t destination, uint8_t channelPage, uint8_t channel, uint16_t macTxUcastTotal, uint16_t macTxUcastFailures, uint16_t macTxUcastRetries, uint8_t period)

Send a request to change the channel to the server by Mgmt_NWK_Unsolicited_Enhanced_Update_notify command.

bool
void

Ignore the SuspendZclMessages command.

API Documentation#

sl_zigbee_af_sub_ghz_client_send_get_suspend_zcl_messages_status_command#

sl_status_t sl_zigbee_af_sub_ghz_client_send_get_suspend_zcl_messages_status_command (sl_802154_short_addr_t nodeId, uint8_t endpoint)

Send the 'Get Suspend ZCL Messages Status' command.

Parameters
TypeDirectionArgument NameDescription
sl_802154_short_addr_tN/AnodeId

The server's node ID.

uint8_tN/Aendpoint

The server's endpoint.

This is a client command. The client sends it to determine the current status of its ZCL communications from the server.


sl_zigbee_af_sub_ghz_client_send_unsolicited_enhanced_update_notify#

sl_status_t sl_zigbee_af_sub_ghz_client_send_unsolicited_enhanced_update_notify (sl_802154_short_addr_t destination, uint8_t channelPage, uint8_t channel, uint16_t macTxUcastTotal, uint16_t macTxUcastFailures, uint16_t macTxUcastRetries, uint8_t period)

Send a request to change the channel to the server by Mgmt_NWK_Unsolicited_Enhanced_Update_notify command.

Parameters
TypeDirectionArgument NameDescription
sl_802154_short_addr_tN/Adestination

........ the Sub-GHz server's node ID

uint8_tN/AchannelPage

........ current channel page

uint8_tN/Achannel

............ current channel

  • the application needs to keep track of these values

uint16_tN/AmacTxUcastTotal

.... total number of Mac TX transaction attempts

uint16_tN/AmacTxUcastFailures

. total number of Mac TX transaction failures

uint16_tN/AmacTxUcastRetries

.. total number of Mac TX transaction retries

uint8_tN/Aperiod

............. time in minutes over which macTxUcastXxx were measured

Returns

  • An ::sl_status_t value.

    • ::SL_STATUS_OK

    • ::SL_STATUS_INVALID_PARAMETER if the channel page or channel are not in the valid range

    • ::SL_STATUS_ALLOCATION_FAILED

    • ::SL_STATUS_NETWORK_DOWN

    • ::SL_STATUS_BUSY


sl_zigbee_af_sub_ghz_client_is_sending_zcl_messages_suspended#

bool sl_zigbee_af_sub_ghz_client_is_sending_zcl_messages_suspended ()

Return the current suspend status.

Returns

  • True if called within a suspend period, false otherwise.


sl_zigbee_af_sub_ghz_client_ignore_suspend_zcl_messages_command#

void sl_zigbee_af_sub_ghz_client_ignore_suspend_zcl_messages_command (bool ignore)

Ignore the SuspendZclMessages command.

Parameters
TypeDirectionArgument NameDescription
boolN/Aignore

True to ignore, false to switch back to normal behavior.

When the client receives the SuspendZclMessages command, it suspends sending any ZCL messages for a given time. This function allows the client to ignore the command and continue sending messages even when suspended.

NOTE: For testing only. Ignoring the SuspendZclMessages command in production is non-compliant.