Sidewalk phy fsk modulation parameters.
Public Attribute Documentation#
freq_dev#
uint32_t sid_pal_radio_fsk_modulation_params_t::freq_dev
Frequency deviation for the FSK modulation
header_type#
enum sid_pal_radio_fsk_header_type sid_pal_radio_fsk_modulation_params_t::header_type
FSK header type
custom_rate_idx#
uint8_t sid_pal_radio_fsk_modulation_params_t::custom_rate_idx
Rate index if the data rate is custom