You are viewing documentation for version:
Sidewalk phy fsk packet parameters.
Public Attribute Documentation#
preamble_length#
uint16_t sid_pal_radio_fsk_packet_params_t::preamble_length
Length of the preamble
preamble_min_detect#
uint8_t sid_pal_radio_fsk_packet_params_t::preamble_min_detect
Minimum preamble detection
sync_word_length#
uint8_t sid_pal_radio_fsk_packet_params_t::sync_word_length
Length of the sync word
addr_comp#
uint8_t sid_pal_radio_fsk_packet_params_t::addr_comp
Address comparison mode
header_type
uint8_t sid_pal_radio_fsk_packet_params_t::header_type
Type of the header
payload_length#
uint8_t sid_pal_radio_fsk_packet_params_t::payload_length
Length of the payload
payload#
uint8_t* sid_pal_radio_fsk_packet_params_t::payload
Pointer to the payload
crc_type#
uint8_t sid_pal_radio_fsk_packet_params_t::crc_type
Type of the CRC
radio_whitening_mode#
uint8_t sid_pal_radio_fsk_packet_params_t::radio_whitening_mode
Radio whitening mode