Bluetooth Mesh On-demand Private Proxy Client Model#
Bluetooth Mesh On-demand Private Proxy Client Model.
The On-Demand Private Proxy Client model is used to configure a node to advertise with Private Network Identity
Modules#
sl_btmesh_evt_on_demand_private_proxy_client_private_gatt_proxy_status
Functions#
Macros#
Function Documentation#
sl_btmesh_on_demand_private_proxy_client_init#
sl_status_t sl_btmesh_on_demand_private_proxy_client_init ()
Initialize the On-Demand Private Proxy Client model
Returns
SL_STATUS_OK if successful. Error code otherwise.
sl_btmesh_on_demand_private_proxy_client_deinit#
sl_status_t sl_btmesh_on_demand_private_proxy_client_deinit ()
Deinitialize the On-Demand Private Proxy Client model
Returns
SL_STATUS_OK if successful. Error code otherwise.
sl_btmesh_on_demand_private_proxy_client_get_on_demand_private_gatt_proxy#
sl_status_t sl_btmesh_on_demand_private_proxy_client_get_on_demand_private_gatt_proxy (uint16_t enc_netkey_index, uint16_t server_address, uint32_t * handle)
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| uint16_t | [in] | enc_netkey_index | Network key used to encrypt the request on the network layer  | 
| uint16_t | [in] | server_address | Destination node primary element address  | 
| uint32_t * | [out] | handle | Request handle  | 
Get node On-Demand Private GATT proxy state.
Returns
SL_STATUS_OK if successful. Error code otherwise.
Events
sl_btmesh_on_demand_private_proxy_client_set_on_demand_private_gatt_proxy#
sl_status_t sl_btmesh_on_demand_private_proxy_client_set_on_demand_private_gatt_proxy (uint16_t enc_netkey_index, uint16_t server_address, uint8_t value, uint32_t * handle)
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| uint16_t | [in] | enc_netkey_index | Network key used to encrypt the request on the network layer  | 
| uint16_t | [in] | server_address | Destination node primary element address  | 
| uint8_t | [in] | value | On-Demand Private GATT proxy value to set. Valid values are: 
  | 
| uint32_t * | [out] | handle | Request handle  | 
Set node On-Demand Private GATT proxy state.
Returns
SL_STATUS_OK if successful. Error code otherwise.
Events