Bluetooth Mesh Configuration Client Model#
Bluetooth Mesh Configuration Client Model.
Bluetooth mesh stack API for the Mesh Configuration Client
Commands in this class configure nodes in the Mesh network, which includes key management, publish and subscribe settings manipulation, and node feature configuration.
Requests to nodes are asynchronous. A handle is assigned to each request that is pending a reply from a node in the network. The handle can be used to query the request status, and to identify the response event from the node. Multiple requests can be made in parallel (as long as they are destined to different nodes; only one pending request per node is allowed).
Request Management
sl_btmesh_config_client_cancel_request : Cancel a request
sl_btmesh_config_client_get_request_status : Query current status of a request
sl_btmesh_config_client_get_default_timeout : Get default request timeout
sl_btmesh_config_client_set_default_timeout : Set default request timeout
Key and Mesh Network Management
sl_btmesh_config_client_add_netkey : Deploy a network key to a node
sl_btmesh_config_client_remove_netkey : Remove a network key from a node
sl_btmesh_config_client_list_netkeys : List network keys on a node
sl_btmesh_config_client_add_appkey : Deploy an application key to a node
sl_btmesh_config_client_remove_appkey : Remove an application key from a node
sl_btmesh_config_client_list_appkeys : List application keys bound to a network key on a node
Node Configuration
sl_btmesh_config_client_get_dcd : Get device composition data of a node
sl_btmesh_config_client_reset_node : Reset a node
sl_btmesh_config_client_get_default_ttl : Get node default TTL state value
sl_btmesh_config_client_set_default_ttl : Set node default TTL state value
sl_btmesh_config_client_get_beacon : Get node secure network beacon state value
sl_btmesh_config_client_set_beacon : Set node secure network beacon state value
sl_btmesh_config_client_get_identity : Get node identity advertising state value
sl_btmesh_config_client_set_identity : Set node identity advertising state value
sl_btmesh_config_client_get_friend : Get node friend state value
sl_btmesh_config_client_set_friend : Set node friend state value
sl_btmesh_config_client_get_lpn_polltimeout : Get node LPN poll timeout state value
sl_btmesh_config_client_get_gatt_proxy : Get node GATT proxy state value
sl_btmesh_config_client_set_gatt_proxy : Set node GATT proxy state value
sl_btmesh_config_client_get_relay : Get node relay state value
sl_btmesh_config_client_set_relay : Set node relay state value
sl_btmesh_config_client_get_network_transmit : Get node network transmit state value
sl_btmesh_config_client_set_network_transmit : Set node network transmit state value
Model Configuration
sl_btmesh_config_client_bind_model : Bind a model to an application key
sl_btmesh_config_client_unbind_model : Remove a model to application key binding
sl_btmesh_config_client_list_bindings : List model to application key bindings on a node
sl_btmesh_config_client_add_model_sub : Add a subscription address to a model
sl_btmesh_config_client_add_model_sub_va : Add a virtual subscription address to a model
sl_btmesh_config_client_remove_model_sub : Remove a subscription address from a model
sl_btmesh_config_client_remove_model_sub_va : Remove a virtual subscription address from a model
sl_btmesh_config_client_set_model_sub : Overwrite the subscription list of a model with an address
sl_btmesh_config_client_set_model_sub_va : Overwrite the subscription list of a model with a virtual address
sl_btmesh_config_client_clear_model_sub : Clear the subscription list of a model
sl_btmesh_config_client_list_subs : Get the subscription list of a model
sl_btmesh_config_client_get_model_pub : Get a model's publication parameters
sl_btmesh_config_client_set_model_pub : Set a model's publication parameters
Heartbeat
sl_btmesh_config_client_get_heartbeat_pub : Get node heartbeat publication settings
sl_btmesh_config_client_set_heartbeat_pub : Set node heartbeat publication settings
sl_btmesh_config_client_get_heartbeat_sub : Get node heartbeat subscription settings
sl_btmesh_config_client_set_heartbeat_sub : Set node heartbeat subscription settings
Modules#
sl_btmesh_evt_config_client_request_modified
sl_btmesh_evt_config_client_netkey_status
sl_btmesh_evt_config_client_netkey_list
sl_btmesh_evt_config_client_netkey_list_end
sl_btmesh_evt_config_client_appkey_status
sl_btmesh_evt_config_client_appkey_list
sl_btmesh_evt_config_client_appkey_list_end
sl_btmesh_evt_config_client_binding_status
sl_btmesh_evt_config_client_bindings_list
sl_btmesh_evt_config_client_bindings_list_end
sl_btmesh_evt_config_client_model_pub_status
sl_btmesh_evt_config_client_model_sub_status
sl_btmesh_evt_config_client_subs_list
sl_btmesh_evt_config_client_subs_list_end
sl_btmesh_evt_config_client_heartbeat_pub_status
sl_btmesh_evt_config_client_heartbeat_sub_status
sl_btmesh_evt_config_client_beacon_status
sl_btmesh_evt_config_client_default_ttl_status
sl_btmesh_evt_config_client_gatt_proxy_status
sl_btmesh_evt_config_client_relay_status
sl_btmesh_evt_config_client_network_transmit_status
sl_btmesh_evt_config_client_identity_status
sl_btmesh_evt_config_client_friend_status
sl_btmesh_evt_config_client_key_refresh_phase_status
sl_btmesh_evt_config_client_lpn_polltimeout_status
sl_btmesh_evt_config_client_dcd_data
sl_btmesh_evt_config_client_dcd_data_end
sl_btmesh_evt_config_client_reset_status
sl_btmesh_evt_config_client_obo_ack_received
Functions#
Macros#
Function Documentation#
sl_btmesh_config_client_cancel_request#
sl_status_t sl_btmesh_config_client_cancel_request (uint32_t handle)
[in] | handle | Request handle |
Cancel an ongoing request releasing resources allocated at the Configuration Client. Note that this call does no undo any setting a node may have made if it had received the request already.
Returns
SL_STATUS_OK if successful. Error code otherwise.
8915
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
sl_btmesh_config_client_get_request_status#
sl_status_t sl_btmesh_config_client_get_request_status (uint32_t handle, uint16_t * server_address, uint16_t * opcode, uint32_t * age_ms, uint32_t * remaining_ms, uint8_t * friend_acked)
[in] | handle | Request handle |
[out] | server_address | Address of the Configuration Server |
[out] | opcode | Message opcode used in the request. Opcodes are defined in the Bluetooth mesh stack 1.0 specification. |
[out] | age_ms | Time in milliseconds that the request has been pending |
[out] | remaining_ms | Time in milliseconds before the request times out. Note that timeout may be adjusted if it's determined that the request is destined to an LPN, which may respond very slowly. |
[out] | friend_acked | If non-zero, response has been acknowledged by a Friend node, so it is destined to an LPN and may take a long time to complete. |
Get the status of a pending request.
Returns
SL_STATUS_OK if successful. Error code otherwise.
8936
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
sl_btmesh_config_client_get_default_timeout#
sl_status_t sl_btmesh_config_client_get_default_timeout (uint32_t * timeout_ms, uint32_t * lpn_timeout_ms)
[out] | timeout_ms | Timeout in milliseconds. Default timeout is 5 s (5000 ms). |
[out] | lpn_timeout_ms | Timeout in milliseconds when communicating with an LPN node. Default LPN timeout is 120 s (120000 ms). |
Get the default timeout for the configuration client requests. If there is no response when the timeout expires, a configuration request is considered to have failed and an event with an error result will be generated. Note that, if the Bluetooth mesh stack notices the request is destined to an LPN by receiving an on-behalf-of acknowledgment from a Friend node, the timeout in use will be changed to the LPN default timeout.
Returns
SL_STATUS_OK if successful. Error code otherwise.
8960
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
sl_btmesh_config_client_set_default_timeout#
sl_status_t sl_btmesh_config_client_set_default_timeout (uint32_t timeout_ms, uint32_t lpn_timeout_ms)
[in] | timeout_ms | Timeout in milliseconds. Default timeout is 5 s (5000 ms). |
[in] | lpn_timeout_ms | Timeout in milliseconds when communicating with an LPN node. Default LPN timeout is 120 s (120000 ms). |
Set the default timeout for the configuration client requests.
Returns
SL_STATUS_OK if successful. Error code otherwise.
8975
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
sl_btmesh_config_client_add_netkey#
sl_status_t sl_btmesh_config_client_add_netkey (uint16_t enc_netkey_index, uint16_t server_address, uint16_t netkey_index, uint32_t * handle)
[in] | enc_netkey_index | Network key used to encrypt the request on the network layer |
[in] | server_address | Destination node primary element address |
[in] | netkey_index | Index of the network key to add |
[out] | handle | Request handle |
Add a network key to a node.
Returns
SL_STATUS_OK if successful. Error code otherwise.
Events
8994
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
sl_btmesh_config_client_remove_netkey#
sl_status_t sl_btmesh_config_client_remove_netkey (uint16_t enc_netkey_index, uint16_t server_address, uint16_t netkey_index, uint32_t * handle)
[in] | enc_netkey_index | Network key used to encrypt the request on the network layer |
[in] | server_address | Destination node primary element address |
[in] | netkey_index | Index of the network key to remove |
[out] | handle | Request handle |
Remove a network key from a node.
Returns
SL_STATUS_OK if successful. Error code otherwise.
Events
9015
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
sl_btmesh_config_client_list_netkeys#
sl_status_t sl_btmesh_config_client_list_netkeys (uint16_t enc_netkey_index, uint16_t server_address, uint32_t * handle)
[in] | enc_netkey_index | Network key used to encrypt the request on the network layer |
[in] | server_address | Destination node primary element address |
[out] | handle | Request handle |
List the network keys on a node.
Returns
SL_STATUS_OK if successful. Error code otherwise.
Events
9036
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
sl_btmesh_config_client_add_appkey#
sl_status_t sl_btmesh_config_client_add_appkey (uint16_t enc_netkey_index, uint16_t server_address, uint16_t appkey_index, uint16_t netkey_index, uint32_t * handle)
[in] | enc_netkey_index | Network key used to encrypt the request on the network layer |
[in] | server_address | Destination node primary element address |
[in] | appkey_index | Index of the application key to add |
[in] | netkey_index | Index of the network key to bind the application key to on the node. Note that this may be different from the binding on other nodes or on the Configuration Client if desired. |
[out] | handle | Request handle |
Add an application key to a node.
Returns
SL_STATUS_OK if successful. Error code otherwise.
Events
9059
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
sl_btmesh_config_client_remove_appkey#
sl_status_t sl_btmesh_config_client_remove_appkey (uint16_t enc_netkey_index, uint16_t server_address, uint16_t appkey_index, uint16_t netkey_index, uint32_t * handle)
[in] | enc_netkey_index | Network key used to encrypt the request on the network layer |
[in] | server_address | Destination node primary element address |
[in] | appkey_index | Index of the application key to remove |
[in] | netkey_index | Index of the network key bound to the application key to on the node. Note that this may be different from the binding on other nodes or on the Configuration Client. |
[out] | handle | Request handle |
Remove an application key from a node.
Returns
SL_STATUS_OK if successful. Error code otherwise.
Events
9084
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
sl_btmesh_config_client_list_appkeys#
sl_status_t sl_btmesh_config_client_list_appkeys (uint16_t enc_netkey_index, uint16_t server_address, uint16_t netkey_index, uint32_t * handle)
[in] | enc_netkey_index | Network key used to encrypt the request on the network layer |
[in] | server_address | Destination node primary element address |
[in] | netkey_index | Network key index for the key used as the query parameter. The result contains the indices of the application keys bound to this network key on the node. |
[out] | handle | Request handle |
List the application keys on a node.
Returns
SL_STATUS_OK if successful. Error code otherwise.
Events
9109
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
sl_btmesh_config_client_bind_model#
sl_status_t sl_btmesh_config_client_bind_model (uint16_t enc_netkey_index, uint16_t server_address, uint8_t elem_index, uint16_t vendor_id, uint16_t model_id, uint16_t appkey_index, uint32_t * handle)
[in] | enc_netkey_index | Network key used to encrypt the request on the network layer |
[in] | server_address | Destination node primary element address |
[in] | elem_index | Index of the element where the model to be configured resides on the node |
[in] | vendor_id | Vendor ID for the model to configure. Use 0xFFFF for Bluetooth SIG models. |
[in] | model_id | Model ID for the model to configure |
[in] | appkey_index | Index of the application key to bind to the model |
[out] | handle | Request handle |
Bind an application key to a model.
Returns
SL_STATUS_OK if successful. Error code otherwise.
Events
9135
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
sl_btmesh_config_client_unbind_model#
sl_status_t sl_btmesh_config_client_unbind_model (uint16_t enc_netkey_index, uint16_t server_address, uint8_t elem_index, uint16_t vendor_id, uint16_t model_id, uint16_t appkey_index, uint32_t * handle)
[in] | enc_netkey_index | Network key used to encrypt the request on the network layer |
[in] | server_address | Destination node primary element address |
[in] | elem_index | Index of the element where the model to be configured resides on the node |
[in] | vendor_id | Vendor ID for the model to configure. Use 0xFFFF for Bluetooth SIG models. |
[in] | model_id | Model ID for the model to configure |
[in] | appkey_index | Index of the application key to unbind from the model |
[out] | handle | Request handle |
Unbind an application key from a model
Returns
SL_STATUS_OK if successful. Error code otherwise.
Events
9164
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
sl_btmesh_config_client_list_bindings#
sl_status_t sl_btmesh_config_client_list_bindings (uint16_t enc_netkey_index, uint16_t server_address, uint8_t elem_index, uint16_t vendor_id, uint16_t model_id, uint32_t * handle)
[in] | enc_netkey_index | Network key used to encrypt the request on the network layer |
[in] | server_address | Destination node primary element address |
[in] | elem_index | Index of the element where the model to be queried resides on the node |
[in] | vendor_id | Vendor ID for the model to query. Use 0xFFFF for Bluetooth SIG models. |
[in] | model_id | Model ID for the model to query |
[out] | handle | Request handle |
List application key bindings of a model.
Returns
SL_STATUS_OK if successful. Error code otherwise.
Events
9193
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
sl_btmesh_config_client_get_model_pub#
sl_status_t sl_btmesh_config_client_get_model_pub (uint16_t enc_netkey_index, uint16_t server_address, uint8_t elem_index, uint16_t vendor_id, uint16_t model_id, uint32_t * handle)
[in] | enc_netkey_index | Network key used to encrypt the request on the network layer |
[in] | server_address | Destination node primary element address |
[in] | elem_index | Index of the element where the model to be queried resides on the node |
[in] | vendor_id | Vendor ID for the model to query. Use 0xFFFF for Bluetooth SIG models. |
[in] | model_id | Model ID for the model to query |
[out] | handle | Request handle |
Get the model publication state.
Returns
SL_STATUS_OK if successful. Error code otherwise.
Events
9220
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
sl_btmesh_config_client_set_model_pub#
sl_status_t sl_btmesh_config_client_set_model_pub (uint16_t enc_netkey_index, uint16_t server_address, uint8_t elem_index, uint16_t vendor_id, uint16_t model_id, uint16_t address, uint16_t appkey_index, uint8_t credentials, uint8_t ttl, uint32_t period_ms, uint8_t retransmit_count, uint16_t retransmit_interval_ms, uint32_t * handle)
[in] | enc_netkey_index | Network key used to encrypt the request on the network layer |
[in] | server_address | Destination node primary element address |
[in] | elem_index | Index of the element where the model to be configured resides on the node |
[in] | vendor_id | Vendor ID for the model to configure. Use 0xFFFF for Bluetooth SIG models. |
[in] | model_id | Model ID for the model to configure |
[in] | address | The address to publish to. It can be a unicast address, a virtual address, or a group address. It can also be the unassigned address to stop the model from publishing. |
[in] | appkey_index | The application key index to use for the published messages. |
[in] | credentials | Friendship credential flag. If zero, publication is done using normal credentials. If one, it is done with friendship credentials, meaning only the friend can decrypt the published message and relay it forward using the normal credentials. The default value is 0. |
[in] | ttl | Publication time-to-live value. Valid values: range[0 - 127] and 255. |
[in] | period_ms | Publication period in milliseconds. Note that the resolution of the publication period is limited by the specification to 100 ms up to a period of 6.3 s, 1 s up to a period of 63 s, 10 s up to a period of 630 s, and 10 minutes above that. Maximum period allowed is 630 minutes. |
[in] | retransmit_count | Publication retransmission count. Valid values range from 0 to 7. |
[in] | retransmit_interval_ms | Publication retransmission interval in millisecond units. The range of value is 50 to 1600 ms, and the resolution of the value is 50 milliseconds. |
[out] | handle | Request handle |
Set the model publication state.
Returns
SL_STATUS_OK if successful. Error code otherwise.
Events
9267
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
sl_btmesh_config_client_set_model_pub_va#
sl_status_t sl_btmesh_config_client_set_model_pub_va (uint16_t enc_netkey_index, uint16_t server_address, uint8_t elem_index, uint16_t vendor_id, uint16_t model_id, uuid_128 address, uint16_t appkey_index, uint8_t credentials, uint8_t ttl, uint32_t period_ms, uint8_t retransmit_count, uint16_t retransmit_interval_ms, uint32_t * handle)
[in] | enc_netkey_index | Network key used to encrypt the request on the network layer |
[in] | server_address | Destination node primary element address |
[in] | elem_index | Index of the element where the model to be configured resides on the node |
[in] | vendor_id | Vendor ID for the model to configure. Use 0xFFFF for Bluetooth SIG models. |
[in] | model_id | Model ID for the model to configure |
[in] | address | The Label UUID (full virtual address) to publish to |
[in] | appkey_index | The application key index to use for the published messages |
[in] | credentials | Friendship credential flag. If zero, publication is done using normal credentials. If one, it is done with friendship credentials, meaning only the friend can decrypt the published message and relay it forward using the normal credentials. The default value is 0. |
[in] | ttl | Publication time-to-live value. Valid values: range[0 - 127] and 255. |
[in] | period_ms | Publication period in milliseconds. Note that the resolution of the publication period is limited by the specification to 100 ms up to a period of 6.3 s, 1 s up to a period of 63 s, 10 s up to a period of 630 s, and 10 minutes above that. Maximum period allowed is 630 minutes. |
[in] | retransmit_count | Publication retransmission count. Valid values range from 0 to 7. |
[in] | retransmit_interval_ms | Publication retransmission interval in millisecond units. The range of value is 50 to 1600 ms. The resolution of the value is 50 milliseconds. |
[out] | handle | Request handle |
Set the model publication state with a full virtual publication address.
Returns
SL_STATUS_OK if successful. Error code otherwise.
Events
9319
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
sl_btmesh_config_client_add_model_sub#
sl_status_t sl_btmesh_config_client_add_model_sub (uint16_t enc_netkey_index, uint16_t server_address, uint8_t elem_index, uint16_t vendor_id, uint16_t model_id, uint16_t sub_address, uint32_t * handle)
[in] | enc_netkey_index | Network key used to encrypt the request on the network layer |
[in] | server_address | Destination node primary element address |
[in] | elem_index | Index of the element where the model, which is about to be configured resides on the node |
[in] | vendor_id | Vendor ID for the model to configure. Use 0xFFFF for Bluetooth SIG models. |
[in] | model_id | Model ID for the model to configure |
[in] | sub_address | The address to add to the subscription list. Note that the address has to be a group address. |
[out] | handle | Request handle |
Add an address to the model subscription list.
Returns
SL_STATUS_OK if successful. Error code otherwise.
Events
9355
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
sl_btmesh_config_client_add_model_sub_va#
sl_status_t sl_btmesh_config_client_add_model_sub_va (uint16_t enc_netkey_index, uint16_t server_address, uint8_t elem_index, uint16_t vendor_id, uint16_t model_id, uuid_128 sub_address, uint32_t * handle)
[in] | enc_netkey_index | Network key used to encrypt the request on the network layer |
[in] | server_address | Destination node primary element address |
[in] | elem_index | Index of the element where the model, which is about to be configured resides on the node |
[in] | vendor_id | Vendor ID for the model to configure. Use 0xFFFF for Bluetooth SIG models. |
[in] | model_id | Model ID for the model to configure |
[in] | sub_address | The full virtual address to add to the subscription list |
[out] | handle | Request handle |
Add a Label UUID (full virtual address) to the model subscription list.
Returns
SL_STATUS_OK if successful. Error code otherwise.
Events
9385
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
sl_btmesh_config_client_remove_model_sub#
sl_status_t sl_btmesh_config_client_remove_model_sub (uint16_t enc_netkey_index, uint16_t server_address, uint8_t elem_index, uint16_t vendor_id, uint16_t model_id, uint16_t sub_address, uint32_t * handle)
[in] | enc_netkey_index | Network key used to encrypt the request on the network layer |
[in] | server_address | Destination node primary element address |
[in] | elem_index | Index of the element where the model, which is about to be configured resides on the node |
[in] | vendor_id | Vendor ID for the model to configure. Use 0xFFFF for Bluetooth SIG models. |
[in] | model_id | Model ID for the model to configure |
[in] | sub_address | The address to remove from the subscription list |
[out] | handle | Request handle |
Remove an address from the model subscription list.
Returns
SL_STATUS_OK if successful. Error code otherwise.
Events
9414
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
sl_btmesh_config_client_remove_model_sub_va#
sl_status_t sl_btmesh_config_client_remove_model_sub_va (uint16_t enc_netkey_index, uint16_t server_address, uint8_t elem_index, uint16_t vendor_id, uint16_t model_id, uuid_128 sub_address, uint32_t * handle)
[in] | enc_netkey_index | Network key used to encrypt the request on the network layer |
[in] | server_address | Destination node primary element address |
[in] | elem_index | Index of the element where the model to be configured resides on the node |
[in] | vendor_id | Vendor ID for the model to configure. Use 0xFFFF for Bluetooth SIG models. |
[in] | model_id | Model ID for the model to configure |
[in] | sub_address | The full virtual address to remove from the subscription list |
[out] | handle | Request handle |
Remove a Label UUID (full virtual address) from the model subscription list.
Returns
SL_STATUS_OK if successful. Error code otherwise.
Events
9444
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
sl_btmesh_config_client_set_model_sub#
sl_status_t sl_btmesh_config_client_set_model_sub (uint16_t enc_netkey_index, uint16_t server_address, uint8_t elem_index, uint16_t vendor_id, uint16_t model_id, uint16_t sub_address, uint32_t * handle)
[in] | enc_netkey_index | Network key used to encrypt the request on the network layer |
[in] | server_address | Destination node primary element address |
[in] | elem_index | Index of the element where the model, which is about to be configured resides on the node |
[in] | vendor_id | Vendor ID for the model to configure. Use 0xFFFF for Bluetooth SIG models. |
[in] | model_id | Model ID for the model to configure |
[in] | sub_address | The address to set as the subscription list |
[out] | handle | Request handle |
Set (overwrite) model subscription address list to a single address.
Returns
SL_STATUS_OK if successful. Error code otherwise.
Events
9473
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
sl_btmesh_config_client_set_model_sub_va#
sl_status_t sl_btmesh_config_client_set_model_sub_va (uint16_t enc_netkey_index, uint16_t server_address, uint8_t elem_index, uint16_t vendor_id, uint16_t model_id, uuid_128 sub_address, uint32_t * handle)
[in] | enc_netkey_index | Network key used to encrypt the request on the network layer |
[in] | server_address | Destination node primary element address |
[in] | elem_index | Index of the element where the model, which is about to be configured resides on the node |
[in] | vendor_id | Vendor ID for the model to configure. Use 0xFFFF for Bluetooth SIG models. |
[in] | model_id | Model ID for the model to configure |
[in] | sub_address | The full virtual address to set as the subscription list |
[out] | handle | Request handle |
Set (overwrite) model subscription address list to a single virtual address.
Returns
SL_STATUS_OK if successful. Error code otherwise.
Events
9503
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
sl_btmesh_config_client_clear_model_sub#
sl_status_t sl_btmesh_config_client_clear_model_sub (uint16_t enc_netkey_index, uint16_t server_address, uint8_t elem_index, uint16_t vendor_id, uint16_t model_id, uint32_t * handle)
[in] | enc_netkey_index | Network key used to encrypt the request on the network layer |
[in] | server_address | Destination node primary element address |
[in] | elem_index | Index of the element where the model, which is about to be configured resides on the node |
[in] | vendor_id | Vendor ID for the model to configure. Use 0xFFFF for Bluetooth SIG models. |
[in] | model_id | Model ID for the model to configure |
[out] | handle | Request handle |
Clear (empty) the model subscription address list.
Returns
SL_STATUS_OK if successful. Error code otherwise.
Events
9531
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
sl_btmesh_config_client_list_subs#
sl_status_t sl_btmesh_config_client_list_subs (uint16_t enc_netkey_index, uint16_t server_address, uint8_t elem_index, uint16_t vendor_id, uint16_t model_id, uint32_t * handle)
[in] | enc_netkey_index | Network key used to encrypt the request on the network layer |
[in] | server_address | Destination node primary element address |
[in] | elem_index | Index of the element where the model, which is about to be queried resides on the node |
[in] | vendor_id | Vendor ID for the model to query. Use 0xFFFF for Bluetooth SIG models. |
[in] | model_id | Model ID for the model to query |
[out] | handle | Request handle |
Get the subscription address list of a model.
Returns
SL_STATUS_OK if successful. Error code otherwise.
Events
9559
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
sl_btmesh_config_client_get_heartbeat_pub#
sl_status_t sl_btmesh_config_client_get_heartbeat_pub (uint16_t enc_netkey_index, uint16_t server_address, uint32_t * handle)
[in] | enc_netkey_index | Network key used to encrypt the request on the network layer |
[in] | server_address | Destination node primary element address |
[out] | handle | Request handle |
Get the heartbeat publication state of a node.
Returns
SL_STATUS_OK if successful. Error code otherwise.
Events
9581
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
sl_btmesh_config_client_set_heartbeat_pub#
sl_status_t sl_btmesh_config_client_set_heartbeat_pub (uint16_t enc_netkey_index, uint16_t server_address, uint16_t destination_address, uint16_t netkey_index, uint8_t count_log, uint8_t period_log, uint8_t ttl, uint16_t features, uint32_t * handle)
[in] | enc_netkey_index | Network key used to encrypt the request on the network layer |
[in] | server_address | Destination node primary element address |
[in] | destination_address | Heartbeat publication destination address. The address can't be a virtual address. Note that it can be the unassigned address, in which case the heartbeat publishing is disabled. |
[in] | netkey_index | Index of the network key used to encrypt heartbeat messages |
[in] | count_log | Heartbeat publication count logarithm-of-2 setting. Valid values are as follows:
|
[in] | period_log | Heartbeat publication period logarithm-of-2 setting. Valid values are as follows:
|
[in] | ttl | Time-to-live value for heartbeat messages |
[in] | features | Heartbeat trigger setting. For bits set in the bitmask, reconfiguration of the node feature associated with the bit will result in the node emitting a heartbeat message. Valid values are as follows:
Remaining bits are reserved for future use. |
[out] | handle | Request handle |
Set the heartbeat publication state of a node.
Returns
SL_STATUS_OK if successful. Error code otherwise.
Events
9629
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
sl_btmesh_config_client_get_heartbeat_sub#
sl_status_t sl_btmesh_config_client_get_heartbeat_sub (uint16_t enc_netkey_index, uint16_t server_address, uint32_t * handle)
[in] | enc_netkey_index | Network key used to encrypt the request on the network layer |
[in] | server_address | Destination node primary element address |
[out] | handle | Request handle |
Get the heartbeat subscription state of a node.
Returns
SL_STATUS_OK if successful. Error code otherwise.
Events
9654
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
sl_btmesh_config_client_set_heartbeat_sub#
sl_status_t sl_btmesh_config_client_set_heartbeat_sub (uint16_t enc_netkey_index, uint16_t server_address, uint16_t source_address, uint16_t destination_address, uint8_t period_log, uint32_t * handle)
[in] | enc_netkey_index | Network key used to encrypt the request on the network layer |
[in] | server_address | Destination node primary element address |
[in] | source_address | Source address for heartbeat messages, which must be either a unicast address or the unassigned address, in which case heartbeat messages are not processed. |
[in] | destination_address | Destination address for heartbeat messages. The address must be either the unicast address of the primary element of the node, a group address, or the unassigned address. If it is the unassigned address, heartbeat messages are not processed. |
[in] | period_log | Heartbeat subscription period logarithm-of-2 setting. Valid values are as follows:
|
[out] | handle | Request handle |
Set the heartbeat subscription state of a node.
Returns
SL_STATUS_OK if successful. Error code otherwise.
Events
9686
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
sl_btmesh_config_client_get_beacon#
sl_status_t sl_btmesh_config_client_get_beacon (uint16_t enc_netkey_index, uint16_t server_address, uint32_t * handle)
[in] | enc_netkey_index | Network key used to encrypt the request on the network layer |
[in] | server_address | Destination node primary element address |
[out] | handle | Request handle |
Get node secure network beacon state.
Returns
SL_STATUS_OK if successful. Error code otherwise.
Events
9708
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
sl_btmesh_config_client_set_beacon#
sl_status_t sl_btmesh_config_client_set_beacon (uint16_t enc_netkey_index, uint16_t server_address, uint8_t value, uint32_t * handle)
[in] | enc_netkey_index | Network key used to encrypt the request on the network layer |
[in] | server_address | Destination node primary element address |
[in] | value | Secure network beacon value to set. Valid values are:
|
[out] | handle | Request handle |
Set node secure network beacon state.
Returns
SL_STATUS_OK if successful. Error code otherwise.
Events
9730
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
sl_btmesh_config_client_get_default_ttl#
sl_status_t sl_btmesh_config_client_get_default_ttl (uint16_t enc_netkey_index, uint16_t server_address, uint32_t * handle)
[in] | enc_netkey_index | Network key used to encrypt the request on the network layer |
[in] | server_address | Destination node primary element address |
[out] | handle | Request handle |
Get node default TTL state.
Returns
SL_STATUS_OK if successful. Error code otherwise.
Events
9750
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
sl_btmesh_config_client_set_default_ttl#
sl_status_t sl_btmesh_config_client_set_default_ttl (uint16_t enc_netkey_index, uint16_t server_address, uint8_t value, uint32_t * handle)
[in] | enc_netkey_index | Network key used to encrypt the request on the network layer |
[in] | server_address | Destination node primary element address |
[in] | value | Default TTL value. Valid value range is from 2 to 127 for relayed PDUs, and 0 to indicate non-relayed PDUs |
[out] | handle | Request handle |
Set node default TTL state.
Returns
SL_STATUS_OK if successful. Error code otherwise.
Events
9771
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
sl_btmesh_config_client_get_gatt_proxy#
sl_status_t sl_btmesh_config_client_get_gatt_proxy (uint16_t enc_netkey_index, uint16_t server_address, uint32_t * handle)
[in] | enc_netkey_index | Network key used to encrypt the request on the network layer |
[in] | server_address | Destination node primary element address |
[out] | handle | Request handle |
Get node GATT proxy state.
Returns
SL_STATUS_OK if successful. Error code otherwise.
Events
9791
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
sl_btmesh_config_client_set_gatt_proxy#
sl_status_t sl_btmesh_config_client_set_gatt_proxy (uint16_t enc_netkey_index, uint16_t server_address, uint8_t value, uint32_t * handle)
[in] | enc_netkey_index | Network key used to encrypt the request on the network layer |
[in] | server_address | Destination node primary element address |
[in] | value | GATT proxy value to set. Valid values are:
|
[out] | handle | Request handle |
Set node GATT proxy state.
Returns
SL_STATUS_OK if successful. Error code otherwise.
Events
9813
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
sl_btmesh_config_client_get_relay#
sl_status_t sl_btmesh_config_client_get_relay (uint16_t enc_netkey_index, uint16_t server_address, uint32_t * handle)
[in] | enc_netkey_index | Network key used to encrypt the request on the network layer |
[in] | server_address | Destination node primary element address |
[out] | handle | Request handle |
Get node relay state.
Returns
SL_STATUS_OK if successful. Error code otherwise.
Events
9833
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
sl_btmesh_config_client_set_relay#
sl_status_t sl_btmesh_config_client_set_relay (uint16_t enc_netkey_index, uint16_t server_address, uint8_t value, uint8_t retransmit_count, uint16_t retransmit_interval_ms, uint32_t * handle)
[in] | enc_netkey_index | Network key used to encrypt the request on the network layer |
[in] | server_address | Destination node primary element address |
[in] | value | Relay value to set. Valid values are:
|
[in] | retransmit_count | Relay retransmit count. Valid values range from 0 to 7; default value is 0 (no retransmissions). |
[in] | retransmit_interval_ms | Relay retransmit interval in milliseconds. Valid values range from 10 ms to 320 ms, with a resolution of 10 ms. The value is ignored if the retransmission count is set to zero. |
[out] | handle | Request handle |
Set node relay state.
Returns
SL_STATUS_OK if successful. Error code otherwise.
Events
9860
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
sl_btmesh_config_client_get_network_transmit#
sl_status_t sl_btmesh_config_client_get_network_transmit (uint16_t enc_netkey_index, uint16_t server_address, uint32_t * handle)
[in] | enc_netkey_index | Network key used to encrypt the request on the network layer |
[in] | server_address | Destination node primary element address |
[out] | handle | Request handle |
Get node network transmit state.
Returns
SL_STATUS_OK if successful. Error code otherwise.
Events
9882
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
sl_btmesh_config_client_set_network_transmit#
sl_status_t sl_btmesh_config_client_set_network_transmit (uint16_t enc_netkey_index, uint16_t server_address, uint8_t transmit_count, uint16_t transmit_interval_ms, uint32_t * handle)
[in] | enc_netkey_index | Network key used to encrypt the request on the network layer |
[in] | server_address | Destination node primary element address |
[in] | transmit_count | Network transmit count. Valid values range from 1 to 8; default value is 1 (single transmission; no retransmissions). |
[in] | transmit_interval_ms | Network transmit interval in milliseconds. Valid values range from 10 ms to 320 ms, with a resolution of 10 ms. The value is ignored if the transmission count is set to one. |
[out] | handle | Request handle |
Set node network transmit state.
Returns
SL_STATUS_OK if successful. Error code otherwise.
Events
9906
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
sl_btmesh_config_client_get_identity#
sl_status_t sl_btmesh_config_client_get_identity (uint16_t enc_netkey_index, uint16_t server_address, uint16_t netkey_index, uint32_t * handle)
[in] | enc_netkey_index | Network key used to encrypt the request on the network layer |
[in] | server_address | Destination node primary element address |
[in] | netkey_index | Network key index for which the state is queried |
[out] | handle | Request handle |
Get node identity state.
Returns
SL_STATUS_OK if successful. Error code otherwise.
Events
9928
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
sl_btmesh_config_client_set_identity#
sl_status_t sl_btmesh_config_client_set_identity (uint16_t enc_netkey_index, uint16_t server_address, uint16_t netkey_index, uint8_t value, uint32_t * handle)
[in] | enc_netkey_index | Network key used to encrypt the request on the network layer |
[in] | server_address | Destination node primary element address |
[in] | netkey_index | Network key index for which the state is configured |
[in] | value | Identity value to set. Valid values are:
|
[out] | handle | Request handle |
Set node identity state.
Returns
SL_STATUS_OK if successful. Error code otherwise.
Events
9952
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
sl_btmesh_config_client_get_friend#
sl_status_t sl_btmesh_config_client_get_friend (uint16_t enc_netkey_index, uint16_t server_address, uint32_t * handle)
[in] | enc_netkey_index | Network key used to encrypt the request on the network layer |
[in] | server_address | Destination node primary element address |
[out] | handle | Request handle |
Get node friend state.
Returns
SL_STATUS_OK if successful. Error code otherwise.
Events
9973
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
sl_btmesh_config_client_set_friend#
sl_status_t sl_btmesh_config_client_set_friend (uint16_t enc_netkey_index, uint16_t server_address, uint8_t value, uint32_t * handle)
[in] | enc_netkey_index | Network key used to encrypt the request on the network layer |
[in] | server_address | Destination node primary element address |
[in] | value | Friend value to set. Valid values are:
|
[out] | handle | Request handle |
Set node friend state.
Returns
SL_STATUS_OK if successful. Error code otherwise.
Events
9995
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
sl_btmesh_config_client_get_key_refresh_phase#
sl_status_t sl_btmesh_config_client_get_key_refresh_phase (uint16_t enc_netkey_index, uint16_t server_address, uint16_t netkey_index, uint32_t * handle)
[in] | enc_netkey_index | Network key used to encrypt the request on the network layer |
[in] | server_address | Destination node primary element address |
[in] | netkey_index | Network key index for which the state is queried |
[out] | handle | Request handle |
Get node key refresh phase state.
Returns
SL_STATUS_OK if successful. Error code otherwise.
Events
10016
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
sl_btmesh_config_client_get_lpn_polltimeout#
sl_status_t sl_btmesh_config_client_get_lpn_polltimeout (uint16_t enc_netkey_index, uint16_t server_address, uint16_t lpn_address, uint32_t * handle)
[in] | enc_netkey_index | Network key used to encrypt the request on the network layer |
[in] | server_address | Destination node primary element address |
[in] | lpn_address | LPN address |
[out] | handle | Request handle |
Get the LPN poll timeout from a Friend node.
Returns
SL_STATUS_OK if successful. Error code otherwise.
Events
10037
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
sl_btmesh_config_client_get_dcd#
sl_status_t sl_btmesh_config_client_get_dcd (uint16_t enc_netkey_index, uint16_t server_address, uint8_t page, uint32_t * handle)
[in] | enc_netkey_index | Network key used to encrypt the request on the network layer |
[in] | server_address | Destination node primary element address |
[in] | page | Composition data page to query |
[out] | handle | Request handle |
Get composition data of a device.
Returns
SL_STATUS_OK if successful. Error code otherwise.
Events
10059
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
sl_btmesh_config_client_reset_node#
sl_status_t sl_btmesh_config_client_reset_node (uint16_t enc_netkey_index, uint16_t server_address, uint32_t * handle)
[in] | enc_netkey_index | Network key used to encrypt the request on the network layer |
[in] | server_address | Destination node primary element address |
[out] | handle | Request handle |
Request a node to unprovision itself. Use this function when a node is removed from the network.
Returns
SL_STATUS_OK if successful. Error code otherwise.
Events
10080
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
sl_btmesh_config_client_set_request_timeout_for_node#
sl_status_t sl_btmesh_config_client_set_request_timeout_for_node (uint16_t lpn_address, uint16_t timeout_ms)
[in] | lpn_address | Destination LPN node primary element address for which the timeout is to be set. |
[in] | timeout_ms | Timeout in milliseconds. |
Set request timeout for a specific node. Typically low power nodes have longer latencies and default timeout may not be sufficient.
Typically this command is issued after receiving a sl_btmesh_evt_config_client_obo_ack_received event indicating that a message has been placed in the Friend Queue. To get an estimate for the needed timeout, sending a sl_btmesh_config_client_get_lpn_polltimeout request to the Friend is recommended.
Returns
SL_STATUS_OK if successful. Error code otherwise.
Events
10105
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h