sl_btmesh_evt_config_client_subs_list#

This event contains a list of addresses that the queried model subscribes to.

The list is requested using the sl_btmesh_config_client_list_subs command. More than one event may be generated. List contents are terminated by a sl_btmesh_evt_config_client_subs_list_end event. Note that, if the subscription address list entry is a Label UUID (full virtual address), the corresponding virtual address hash is returned in this event.

Modules#

sl_btmesh_evt_config_client_subs_list_s

Macros#

#define
sl_btmesh_evt_config_client_subs_list_id 0x0c2700a8

Identifier of the subs_list event.

Typedef Documentation#

sl_btmesh_evt_config_client_subs_list_t#

typedef struct sl_btmesh_evt_config_client_subs_list_s sl_btmesh_evt_config_client_subs_list_t

Definition at line 8454 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h