Bluetooth Mesh Diagnostic Utilities#
Bluetooth Mesh Diagnostic Utilities.
Diagnostic Utilities. It provides the functionality that assist with diagnosing problems.
Modules#
sl_btmesh_evt_diagnostic_relay
sl_btmesh_evt_diagnostic_friend_queue
sl_btmesh_evt_diagnostic_friend_relay
sl_btmesh_evt_diagnostic_friend_remove
Functions#
Macros#
Function Documentation#
sl_btmesh_diagnostic_init#
sl_status_t sl_btmesh_diagnostic_init ()
Initialize Diagnostic Utilities.
Returns
SL_STATUS_OK if successful. Error code otherwise.
sl_btmesh_diagnostic_deinit#
sl_status_t sl_btmesh_diagnostic_deinit ()
Deinitialize Diagnostic Utilities. After this call it cannot be used until it is initialized again. See sl_btmesh_diagnostic_init.
Returns
SL_STATUS_OK if successful. Error code otherwise.
sl_btmesh_diagnostic_enable_relay#
sl_status_t sl_btmesh_diagnostic_enable_relay ()
Enable event sending for each relayed or proxied message. NOTE: On NCP target this can saturate the NCP PHY interface. An alternative for this is sl_btmesh_diagnostic_get_relay
Returns
SL_STATUS_OK if successful. Error code otherwise.
Events
sl_btmesh_diagnostic_disable_relay#
sl_status_t sl_btmesh_diagnostic_disable_relay ()
Disable event sending for each relayed or proxied message.
Returns
SL_STATUS_OK if successful. Error code otherwise.
sl_btmesh_diagnostic_get_relay#
sl_status_t sl_btmesh_diagnostic_get_relay (uint32_t * relay_counter)
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| uint32_t * | [out] | relay_counter | Relayed or proxied message counter.  | 
Get relayed or proxied message counter, which is a counter incremented for each relayed or proxied message.
Returns
SL_STATUS_OK if successful. Error code otherwise.
sl_btmesh_diagnostic_get_statistics#
sl_status_t sl_btmesh_diagnostic_get_statistics (uint32_t requested_chunk, uint32_t requested_offset, uint32_t * total_length, uint32_t * chunk_offset, size_t max_statistics_size, size_t * statistics_len, uint8_t * statistics)
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| uint32_t | [in] | requested_chunk | Size of the statistics data chunk requested  | 
| uint32_t | [in] | requested_offset | Byte offset to the statistics data chunk requested  | 
| uint32_t * | [out] | total_length | Total length of the statistics data in the system  | 
| uint32_t * | [out] | chunk_offset | Byte offset to the statistics data chunk delivered  | 
| size_t | [in] | max_statistics_size | Size of output buffer passed in   | 
| size_t * | [out] | statistics_len | On return, set to the length of output data written to   | 
| uint8_t * | [out] | statistics | Raw statistics data counter array.  | 
Get a chunk of Bluetooth mesh stack statistics data counters. As there can be a large amount of statistics, it has to be retrieved as chunks. The application is free to specify the size of the chunk it wants to use, but keep in mind that for the NCP use case there may be limited size buffers in the underlying serial channel.
Returns
SL_STATUS_OK if successful. Error code otherwise.
sl_btmesh_diagnostic_clear_statistics#
sl_status_t sl_btmesh_diagnostic_clear_statistics ()
Clear Bluetooth mesh stack statistics data counters.
Returns
SL_STATUS_OK if successful. Error code otherwise.
sl_btmesh_diagnostic_enable_friend#
sl_status_t sl_btmesh_diagnostic_enable_friend ()
Enable event sending for friendship diagnostics on the friend node side. NOTE: On NCP target this can saturate the NCP PHY interface. An alternative for this is sl_btmesh_diagnostic_get_friend
Returns
SL_STATUS_OK if successful. Error code otherwise.
Events
sl_btmesh_diagnostic_disable_friend#
sl_status_t sl_btmesh_diagnostic_disable_friend ()
Disable event sending for friendship diagnostics on the friend node side.
Returns
SL_STATUS_OK if successful. Error code otherwise.
sl_btmesh_diagnostic_get_friend#
sl_status_t sl_btmesh_diagnostic_get_friend (uint32_t * queue_counter, uint32_t * relay_counter, uint32_t * remove_counter_sent, uint32_t * remove_counter_old_pdu, uint32_t * remove_counter_old_segack, uint32_t * remove_counter_old_segment)
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| uint32_t * | [out] | queue_counter | Number of messages queued for LPNs.  | 
| uint32_t * | [out] | relay_counter | Number of messages relayed to LPNs as a response to polls.  | 
| uint32_t * | [out] | remove_counter_sent | Number of messages discarded from LPN friendship queues due to message having been to sent to LPN and acknowledged by LPN by it sending the next poll.  | 
| uint32_t * | [out] | remove_counter_old_pdu | Number of messages discarded from LPN friendship queues due to message queue overflow, resulting in the need to flush the oldest PDU un the queue  | 
| uint32_t * | [out] | remove_counter_old_segack | Number of messages discarded from LPN friendship queues due to a new segment acknowledgement message replacing an old one in the queue.  | 
| uint32_t * | [out] | remove_counter_old_segment | Number of messages discarded from LPN friendship queues due to invalidated segments being removed from the queue.  | 
Get friend event counters.
Returns
SL_STATUS_OK if successful. Error code otherwise.