Bluetooth Mesh Vendor Model#
Bluetooth Mesh Vendor Model.
Vendor model API provides functionality to send and receive vendor-specific messages.
Throughout the API, the manipulated model is identified by its element address, vendor ID, and model ID.
The API has functions for sending, receiving, and publishing messages. The application has to implement additional complex functionality (state machines or other model-specific logic).
The stack will handle Mesh transaction layer segmentation and reassembly automatically if the messages sent are long enough to require it.
Note that as the application layer overhead for vendor messages is three bytes (vendor ID and opcode) and the access layer MIC is at least four bytes, the longest vendor application payload which can be sent using an unsegmented transport layer PDU is eight bytes. On the other hand, the longest vendor application payload which can be sent using transport layer segmentation is 377 bytes (fragmented into 32 segments).
Modules#
sl_btmesh_evt_vendor_model_receive
sl_btmesh_evt_vendor_model_send_complete
Enumerations#
Key values to identify vendor model configuration options.
Functions#
Macros#
Enumeration Documentation#
sl_btmesh_vendor_model_options_t#
sl_btmesh_vendor_model_options_t
Key values to identify vendor model configuration options.
| Enumerator | |
|---|---|
| sl_btmesh_vendor_model_heap_work_buffer | (0x0) If set to 1, each vendor model allocates a heap work buffer for messages being received. If set to 0, no heap work buffer allocation is made, which saves memory but risks losing messages in a high load environment. Range: 0...1 Default: 1  | 
Function Documentation#
sl_btmesh_vendor_model_send#
sl_status_t sl_btmesh_vendor_model_send (uint16_t destination_address, int8_t va_index, uint16_t appkey_index, uint16_t elem_index, uint16_t vendor_id, uint16_t model_id, uint8_t nonrelayed, uint8_t opcode, uint8_t final, size_t payload_len, const uint8_t * payload)
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| uint16_t | [in] | destination_address | Destination address of the message. It can be a unicast address, a group address, or a virtual address.  | 
| int8_t | [in] | va_index | Index of the destination Label UUID (used only is the destination address is a virtual address)  | 
| uint16_t | [in] | appkey_index | The application key index used  | 
| uint16_t | [in] | elem_index | Sending model element index  | 
| uint16_t | [in] | vendor_id | Vendor ID of the sending model  | 
| uint16_t | [in] | model_id | Model ID of the sending model  | 
| uint8_t | [in] | nonrelayed | If the message is a response to a received message, set this parameter according to what was received in the receive event. Otherwise, set to non-zero if the message affects only devices in the immediate radio neighborhood.  | 
| uint8_t | [in] | opcode | Message opcode  | 
| uint8_t | [in] | final | Indicates whether this payload chunk is the final one of the message or whether more will follow.  | 
| size_t | [in] | payload_len | Length of data in   | 
| const uint8_t * | [in] | payload | Payload data (either complete or partial; see final parameter).  | 
Send vendor-specific data.
Note that, because of the bgapi event length restrictions, the message sent may need to be fragmented into several commands. If this is the case, the application must issue the commands in the correct order and mark the command carrying the last message fragment with the final flag set to a non-zero value. The stack will not start sending the message until the complete message is provided by the application. Fragments from multiple messages must not be interleaved.
Returns
SL_STATUS_OK if successful. Error code otherwise.
sl_btmesh_vendor_model_set_publication#
sl_status_t sl_btmesh_vendor_model_set_publication (uint16_t elem_index, uint16_t vendor_id, uint16_t model_id, uint8_t opcode, uint8_t final, size_t payload_len, const uint8_t * payload)
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| uint16_t | [in] | elem_index | Publishing model element index  | 
| uint16_t | [in] | vendor_id | Vendor ID of the model  | 
| uint16_t | [in] | model_id | Model ID of the model  | 
| uint8_t | [in] | opcode | Message opcode  | 
| uint8_t | [in] | final | Indicates whether this payload chunk is the final one of the message or whether more will follow.  | 
| size_t | [in] | payload_len | Length of data in   | 
| const uint8_t * | [in] | payload | Payload data (either complete or partial; see final parameter).  | 
Set the vendor model publication message.
The model publication message will be sent out when the model publication occurs either periodically (if the model is configured for periodic publishing) or explicitly (see sl_btmesh_vendor_model_publish.
Note that, because of bgapi length requirements, the message may need to be fragmented over multiple commands. If this is the case, the application must issue the commands in the correct order and mark the command carrying the last message fragment with the final flag set to a non-zero value. The stack will not assign the message to the model until the complete message is provided by the application.
To disable publication, the publication message may be erased using the sl_btmesh_vendor_model_clear_publication command.
Returns
SL_STATUS_OK if successful. Error code otherwise.
sl_btmesh_vendor_model_clear_publication#
sl_status_t sl_btmesh_vendor_model_clear_publication (uint16_t elem_index, uint16_t vendor_id, uint16_t model_id)
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| uint16_t | [in] | elem_index | Publishing model element index  | 
| uint16_t | [in] | vendor_id | Vendor ID of the model  | 
| uint16_t | [in] | model_id | Model ID of the model  | 
Clear the vendor model publication message.
Clearing the model publication message disables model publishing, which can be re-enabled by defining the publication message using the sl_btmesh_vendor_model_set_publication command.
Returns
SL_STATUS_OK if successful. Error code otherwise.
sl_btmesh_vendor_model_publish#
sl_status_t sl_btmesh_vendor_model_publish (uint16_t elem_index, uint16_t vendor_id, uint16_t model_id)
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| uint16_t | [in] | elem_index | Publishing model element index  | 
| uint16_t | [in] | vendor_id | Vendor ID of the model  | 
| uint16_t | [in] | model_id | Model ID of the model  | 
Publish the vendor model publication message.
Sends the stored publication message to the network using the application key and destination address stored in the model publication parameters.
Returns
SL_STATUS_OK if successful. Error code otherwise.
sl_btmesh_vendor_model_init#
sl_status_t sl_btmesh_vendor_model_init (uint16_t elem_index, uint16_t vendor_id, uint16_t model_id, uint8_t publish, size_t opcodes_len, const uint8_t * opcodes)
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| uint16_t | [in] | elem_index | Model element index  | 
| uint16_t | [in] | vendor_id | Vendor ID of the model  | 
| uint16_t | [in] | model_id | Model ID of the model  | 
| uint8_t | [in] | publish | Indicates if the model is a publish model (non-zero) or not (zero).  | 
| size_t | [in] | opcodes_len | Length of data in   | 
| const uint8_t * | [in] | opcodes | Array of opcodes the model can handle  | 
Initialize the vendor model. This function has to be called before the model can be used. Note that the model can be deinitialized if it is no longer needed. See sl_btmesh_vendor_model_deinit.
Opcodes that the model is able to receive at initialization must be defined. This enables the stack to pass only valid messages up to the model during runtime. Per Mesh specification there are up to 64 opcodes per vendor, ranging from 0 to 63. Specifying opcodes outside of that range will result in an error response. Duplicate opcodes in the array do not result in an error, but will of course be recorded only once.
Returns
SL_STATUS_OK if successful. Error code otherwise.
sl_btmesh_vendor_model_deinit#
sl_status_t sl_btmesh_vendor_model_deinit (uint16_t elem_index, uint16_t vendor_id, uint16_t model_id)
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| uint16_t | [in] | elem_index | Model element index  | 
| uint16_t | [in] | vendor_id | Vendor ID of the model  | 
| uint16_t | [in] | model_id | Model ID of the model  | 
Deinitialize the model. After this call, the model cannot be used until it is initialized again. See sl_btmesh_vendor_model_init.
Returns
SL_STATUS_OK if successful. Error code otherwise.
sl_btmesh_vendor_model_send_tracked#
sl_status_t sl_btmesh_vendor_model_send_tracked (uint16_t destination_address, int8_t va_index, uint16_t appkey_index, uint16_t elem_index, uint16_t vendor_id, uint16_t model_id, uint8_t nonrelayed, uint8_t segment, uint8_t opcode, uint8_t final, size_t payload_len, const uint8_t * payload, uint16_t * handle)
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| uint16_t | [in] | destination_address | Destination address of the message. It can be a unicast address, a group address, or a virtual address.  | 
| int8_t | [in] | va_index | Index of the destination Label UUID (used only is the destination address is a virtual address)  | 
| uint16_t | [in] | appkey_index | The application key index used  | 
| uint16_t | [in] | elem_index | Sending model element index  | 
| uint16_t | [in] | vendor_id | Vendor ID of the sending model  | 
| uint16_t | [in] | model_id | Model ID of the sending model  | 
| uint8_t | [in] | nonrelayed | If the message is a response to a received message, set this parameter according to what was received in the receive event. Otherwise, set to non-zero if the message affects only devices in the immediate radio neighborhood.  | 
| uint8_t | [in] | segment | If nonzero, instruct the stack to use transport layer segmentation, even if the data would be short enough to send as an unsegmented message. If zero, stack selects automatically based on data length whether to use segmentation or not.  | 
| uint8_t | [in] | opcode | Message opcode  | 
| uint8_t | [in] | final | Indicates whether this payload chunk is the final one of the message or whether more will follow.  | 
| size_t | [in] | payload_len | Length of data in   | 
| const uint8_t * | [in] | payload | Payload data (either complete or partial; see final parameter).  | 
| uint16_t * | [out] | handle | Tracking handle for the message sending. Note that a valid handle is returned only when the final payload fragment is received by the stack (as indicated by the final parameter of this message) and the message is accepted for delivery (as indicated by the result code). Otherwise the value of this parameter should be ignored.  | 
Send vendor-specific data with a delivery report.
This command works otherwise as sl_btmesh_vendor_model_send but also provides a tracking handle if there is no immediate local error. Once the message sending completes a sl_btmesh_evt_vendor_model_send_complete event is generated, and the handle received here can be used to correlate the event to the sent message.
Returns
SL_STATUS_OK if successful. Error code otherwise.
sl_btmesh_vendor_model_set_publication_tracked#
sl_status_t sl_btmesh_vendor_model_set_publication_tracked (uint16_t elem_index, uint16_t vendor_id, uint16_t model_id, uint8_t segment, uint8_t opcode, uint8_t final, size_t payload_len, const uint8_t * payload, uint16_t * handle)
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| uint16_t | [in] | elem_index | Publishing model element index  | 
| uint16_t | [in] | vendor_id | Vendor ID of the model  | 
| uint16_t | [in] | model_id | Model ID of the model  | 
| uint8_t | [in] | segment | If nonzero, instruct the stack to use transport layer segmentation, even if the data would be short enough to publish as an unsegmented message. If zero, stack selects automatically based on data length whether to use segmentation or not.  | 
| uint8_t | [in] | opcode | Message opcode  | 
| uint8_t | [in] | final | Indicates whether this payload chunk is the final one of the message or whether more will follow.  | 
| size_t | [in] | payload_len | Length of data in   | 
| const uint8_t * | [in] | payload | Payload data (either complete or partial; see final parameter).  | 
| uint16_t * | [out] | handle | Tracking handle for the message publishing. Note that a valid handle is returned only when the final payload fragment is received by the stack (as indicated by the final parameter of this message) and the message is accepted for publication (as indicated by the result code). Otherwise the value of this parameter should be ignored. attempt  | 
Set the vendor model publication message with a delivery report.
This command works otherwise as sl_btmesh_vendor_model_set_publication but also sets up a tracking handle for monitoring message delivery. When the message publishing completes a sl_btmesh_evt_vendor_model_send_complete event is generated, and the handle received here can be used to correlate the event to the sent message.
Note that the same tracking handle will be reported multiple times in case of periodic publication or publication retransmissions.
Returns
SL_STATUS_OK if successful. Error code otherwise.
sl_btmesh_vendor_model_set_option#
sl_status_t sl_btmesh_vendor_model_set_option (uint8_t option, uint32_t value)
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| uint8_t | [in] | option | Enum sl_btmesh_vendor_model_options_t. Configuration option.  | 
| uint32_t | [in] | value | Configuration value  | 
Set global vendor model configuration options.
This command sets global configuration options for all vendor models. Options take effect when models are initialized, so this command should be called before any sl_btmesh_vendor_model_init call.
Returns
SL_STATUS_OK if successful. Error code otherwise.