sl_btmesh_evt_config_client_model_sub_status#
Status event for sl_btmesh_config_client_add_model_sub : add subscription address, sl_btmesh_config_client_add_model_sub_va : add subscription virtual address, sl_btmesh_config_client_remove_model_sub : remove subscription address, sl_btmesh_config_client_remove_model_sub_va : remove subscription virtual address, sl_btmesh_config_client_set_model_sub : set subscription address, sl_btmesh_config_client_set_model_sub_va : set subscription virtual address, and sl_btmesh_config_client_clear_model_sub : clear subscription address list commands.
Modules#
sl_btmesh_evt_config_client_model_sub_status_s
Typedefs#
Macros#
#define
sl_btmesh_evt_config_client_model_sub_status_id 0x0b2700a8
Identifier of the model_sub_status event.
Typedef Documentation#
sl_btmesh_evt_config_client_model_sub_status_t#
typedef struct sl_btmesh_evt_config_client_model_sub_status_s sl_btmesh_evt_config_client_model_sub_status_t
Definition at line
8425
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h