sl_btmesh_evt_config_client_model_pub_status#

Status event for sl_btmesh_config_client_get_model_pub, sl_btmesh_config_client_set_model_pub, sl_btmesh_config_client_set_model_pub_va commands.

Modules#

sl_btmesh_evt_config_client_model_pub_status_s

Macros#

#define

Identifier of the model_pub_status event.

Typedef Documentation#

sl_btmesh_evt_config_client_model_pub_status_t#

typedef struct sl_btmesh_evt_config_client_model_pub_status_s sl_btmesh_evt_config_client_model_pub_status_t

Definition at line 8395 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

Macro Definition Documentation#

sl_btmesh_evt_config_client_model_pub_status_id#

#define sl_btmesh_evt_config_client_model_pub_status_id
Value:
0x0a2700a8

Identifier of the model_pub_status event.


Definition at line 8368 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h