Data structure of the attention event.

Public Attributes#

uint16_t
uint8_t

Public Attribute Documentation#

elem_index#

uint16_t sl_btmesh_evt_health_server_attention_s::elem_index

Index of the element for which attention timer was set


Definition at line 4886 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

timer_sec#

uint8_t sl_btmesh_evt_health_server_attention_s::timer_sec

Timer value in seconds. If zero, user attention is no longer required.


Definition at line 4888 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h