Data structure of the test_request event.
Public Attribute Documentation#
server_address#
uint16_t sl_btmesh_evt_health_server_test_request_s::server_address
Destination address the message was sent to. It can be either the Server model element's unicast address, or a subscription address of the Server model.
Definition at line
4913
of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
elem_index#
uint16_t sl_btmesh_evt_health_server_test_request_s::elem_index
Server model element index. Identifies the Server model that received the request as well as the element on which the test is to be performed.
Definition at line
4917
of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
client_address#
uint16_t sl_btmesh_evt_health_server_test_request_s::client_address
Address of the client model which sent the message
Definition at line
4921
of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
appkey_index#
uint16_t sl_btmesh_evt_health_server_test_request_s::appkey_index
The application key index to use in encrypting the request. Any response sent must be encrypted using the same key.
Definition at line
4923
of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
test_id#
uint8_t sl_btmesh_evt_health_server_test_request_s::test_id
Test ID
Definition at line
4926
of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
vendor_id#
uint16_t sl_btmesh_evt_health_server_test_request_s::vendor_id
Bluetooth vendor ID used in the request
Definition at line
4927
of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
response_required#
uint8_t sl_btmesh_evt_health_server_test_request_s::response_required
Non-zero if client expects a response. The application should issue a sl_btmesh_health_server_send_test_response once it has processed the request.
Definition at line
4928
of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h