sl_btmesh_evt_lc_setup_server_set_property#

LC Property Set from the Client.

Modules#

sl_btmesh_evt_lc_setup_server_set_property_s

Macros#

#define

Identifier of the set_property event.

Typedef Documentation#

sl_btmesh_evt_lc_setup_server_set_property_t#

typedef struct sl_btmesh_evt_lc_setup_server_set_property_s sl_btmesh_evt_lc_setup_server_set_property_t

Definition at line 14400 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

Macro Definition Documentation#

sl_btmesh_evt_lc_setup_server_set_property_id#

#define sl_btmesh_evt_lc_setup_server_set_property_id
Value:
0x004e00a8

Identifier of the set_property event.


Definition at line 14383 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h