Data structure of the set_property event.

Public Attribute Documentation#

destination_address#

uint16_t sl_btmesh_evt_lc_setup_server_set_property_s::destination_address

Address of the server or the group address to which it was published.


elem_index#

uint16_t sl_btmesh_evt_lc_setup_server_set_property_s::elem_index

Index of the element which received the command.


client_address#

uint16_t sl_btmesh_evt_lc_setup_server_set_property_s::client_address

Device which sent the request.


appkey_index#

uint16_t sl_btmesh_evt_lc_setup_server_set_property_s::appkey_index

Appkey used by client_address.


property_id#

uint16_t sl_btmesh_evt_lc_setup_server_set_property_s::property_id

Property ID


property_value#

uint8array sl_btmesh_evt_lc_setup_server_set_property_s::property_value

Property value