Data structure of the friendship_established event.

Public Attributes#

uint16_t

Public Attribute Documentation#

netkey_index#

uint16_t sl_btmesh_evt_lpn_friendship_established_s::netkey_index

Network key index


Definition at line 7638 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

friend_address#

uint16_t sl_btmesh_evt_lpn_friendship_established_s::friend_address

Friend node address


Definition at line 7639 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h