You are viewing documentation for version:
sl_btmesh_evt_mbt_server_chunk#
Received a new chunk of BLOB data.
Each chunk is delivered to the application with this event only once when it is first received. The offset of the chunk data
relative to the whole BLOB is in total_offset
, and relative to the current block in block_offset
.
Modules#
sl_btmesh_evt_mbt_server_chunk_s
Macros#
#define
Identifier of the chunk event.
Typedef Documentation#
sl_btmesh_evt_mbt_server_chunk_t#
typedef struct sl_btmesh_evt_mbt_server_chunk_s sl_btmesh_evt_mbt_server_chunk_t
Definition at line 11340
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
Macro Definition Documentation#
sl_btmesh_evt_mbt_server_chunk_id#
#define sl_btmesh_evt_mbt_server_chunk_id
Value:0x032900a8
Identifier of the chunk event.
Definition at line 11325
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h