sl_btmesh_evt_mbt_server_transfer_start_req#

The MBT Client has requested the transfer start.

The command sl_btmesh_mbt_server_transfer_start_rsp must be called to accept or reject the transfer start request.

After the transfer has been started, the start of the first block is indicated by the sl_btmesh_evt_mbt_server_block_start event.

Modules#

sl_btmesh_evt_mbt_server_transfer_start_req_s

Macros#

#define

Identifier of the transfer_start_req event.

Typedef Documentation#

sl_btmesh_evt_mbt_server_transfer_start_req_t#

typedef struct sl_btmesh_evt_mbt_server_transfer_start_req_s sl_btmesh_evt_mbt_server_transfer_start_req_t

Definition at line 11277 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

Macro Definition Documentation#

sl_btmesh_evt_mbt_server_transfer_start_req_id#

#define sl_btmesh_evt_mbt_server_transfer_start_req_id
Value:
0x002900a8

Identifier of the transfer_start_req event.


Definition at line 11260 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h