sl_btmesh_evt_node_ivrecovery_needed#

Network IV index recovery needed.

This event is generated when the node detects the network IV index is too far in the future to be automatically updated. See sl_btmesh_node_set_ivrecovery_mode command.

Modules#

sl_btmesh_evt_node_ivrecovery_needed_s

Macros#

#define

Identifier of the ivrecovery_needed event.

Typedef Documentation#

sl_btmesh_evt_node_ivrecovery_needed_t#

typedef struct sl_btmesh_evt_node_ivrecovery_needed_s sl_btmesh_evt_node_ivrecovery_needed_t

Definition at line 699 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

Macro Definition Documentation#

sl_btmesh_evt_node_ivrecovery_needed_id#

#define sl_btmesh_evt_node_ivrecovery_needed_id
Value:
0x0b1400a8

Identifier of the ivrecovery_needed event.


Definition at line 688 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h