sl_btmesh_evt_node_reset#

Provisioner has instructed the node to reset.

This event is generated when the Provisioner has ordered the node to be reset. Stack data has already been reset. This event is generated to inform the application that it should do its own cleanup duties and reset the hardware.

Macros#

#define

Identifier of the reset event.

Macro Definition Documentation#

sl_btmesh_evt_node_reset_id#

#define sl_btmesh_evt_node_reset_id
Value:
0x0a1400a8

Identifier of the reset event.


Definition at line 673 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h